memtool for i.MX6DP processor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

memtool for i.MX6DP processor

9,854件の閲覧回数
saurabh206
Senior Contributor III


Hi,

I want memtool for i.MX6DP processor.

How can I get updated memtool code for i.MX6DP processor.

Thanks

Saurabh

ラベル(3)
タグ(1)
4 返答(返信)

5,764件の閲覧回数
marcocavallini
Contributor V

5,764件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please use the recent BSP, which supports i.MX 6QuadPlus SABRE-SD

Board and Platform.

https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_MX6QDLSOLO&appType=license&location=null

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

5,764件の閲覧回数
saurabh206
Senior Contributor III

Hi Yuri

Thanks for reply.

However I am using 3.154.52 only (imx-test-5.3).

It only provides support for mx6dl, mx6q, mx6sl, mx6sx and mx6ul.

Thanks

Saurabh

0 件の賞賛
返信

5,764件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

the following helps to clarify how to build the unit_tests , including the memtool.

How to include memtool in the core-image-base ?

Please use the recent Linux BSP

i.MX 6 Series Software and Development Tool|NXP

Regards,

Yuri.

0 件の賞賛
返信