memory usage by boot ROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

memory usage by boot ROM

1,522 Views
jameshe1
Contributor II

Hello Yuri

  Do you know where the flash data is loaded to in the system memory? is the address 0x00907000?

0 Kudos
Reply
1 Reply

1,413 Views
Yuri
NXP Employee
NXP Employee

Hello,

You may look at the following regarding SD boot (it is similar to NAND, SPI NOR ones).

How to build bootable SD image (for i.MX6 SL as example) 

 You may look at Chapter 8 (System Boot) of i.MX6 D/Q RM for some details.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply