memory usage by boot ROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

memory usage by boot ROM

1,482件の閲覧回数
jameshe1
Contributor II

Hello Yuri

  Do you know where the flash data is loaded to in the system memory? is the address 0x00907000?

0 件の賞賛
返信
1 返信

1,373件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

You may look at the following regarding SD boot (it is similar to NAND, SPI NOR ones).

How to build bootable SD image (for i.MX6 SL as example) 

 You may look at Chapter 8 (System Boot) of i.MX6 D/Q RM for some details.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信