media player application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

media player application

2,305 Views
Hitex
Fresh Out Contributor

Did any one tried media player application on imx53

I created 3 media player based on

  • Phonon
  • Gstreamer
  • Mplayer

All are working find on X86 system,

However when I tried on imx53 QSB none is working.
I am getting only the sound in imx53

Did any one faced the same problem.


Labels (1)
0 Kudos
Reply
2 Replies

2,198 Views
Hitex
Fresh Out Contributor

Hi Randy,

I am using Ubuntu 10.04 as OS provided by freescale (MX53_QSB_UBUNTU_SD_DEMO_IMAGE )

I guess version is Rev #: 11.09

How I get the logs/errors as in the terminal of QSB after invoking the application I am not getting any message.

Only black screen i get

118-ScreenshotUntitledWindow1.pngOn IMX53 QSB screen

120-ScreenshotUntitledWindow.pngOn x86 machine

Both are Ubuntu10.04 QSB as well as x86

0 Kudos
Reply

2,198 Views
RandyKrakora
NXP Employee
NXP Employee

Do you have any logs of errors? What OS are you running on the imx53 ( ltib build or Ubuntu that came with the QSB )? If Ubuntu, do you know what version it is ( on the card - 11.01/11.03/?? ).

-Randy

0 Kudos
Reply