maximum delay between the write into the ECSPIx_CONFIGREG register and the change of SCLK polarity

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

maximum delay between the write into the ECSPIx_CONFIGREG register and the change of SCLK polarity

1,537 Views
yuuki
Senior Contributor II

Dear all,

We are porting of Linux to our i.MX6 solo board to a base in Linux L3.10.53 BSP.

In our system, Flash and RTC are connected to SPI.

The device connected to SSx of SPI is the following.
SS0: Flash 200MHz
SS1: Flash 200MHz
SS2: RTC 20MHz

With switches from SS2 to SS0, we found SCLK polarity changing after GPIO chipselect was asserted.

We found the following patch about SPI.

http://git.kernel.org/cgit/linux/kernel/git/torvalds/linux.git/commit/?id=6fd8b8503a0dcf66510314dc05...

The contents of this patch are included in Linux L3 .10.53 BSP.
However, this problem does not seem to be solved.

According to Explanation of this patch, the following is explained.
"Therefore, the time it takes for the write to ECSPIx_CONFIGREG to take effect in the hardware is up to the duration of 1 tick of the SCLK clock."

For i.MX6, it seems that the delay time is bigger than 1 tick of the SCLK clock.

Would you tell me the maximum delay between the write into the ECSPIx_CONFIGREG register and the change of SCLK polarity?

It it is the setting that SCLK polarity is not changed, a glitch occurs on SCLK.
https://community.freescale.com/thread/386935

Best Regards,
Yuuki

Labels (2)
0 Kudos
Reply
1 Reply

1,316 Views
art
NXP Employee
NXP Employee

You are right in that the maximum delay between writing to the ECSPIx_CONFIGREG register that changes some SCLK parameters (e.g. SCLK polarity or SCLK idle state) and actual parameter change is one SCLK clock period.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply