manufacturing tool question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

manufacturing tool question

1,418 次查看
sivaci2754
Contributor I

For i.MX 8X EVM Kit usage, Could you please let us know how to use the serial download mode for the Manufacturing tool? It seems to be not enough to understand the procedure of usage.

What kind of tools can be supported in the serial boot mode?  https://tutuappx.com/ Vidmate

0 项奖励
回复
2 回复数

1,398 次查看
ramprakash08
Contributor IV

Hi,

For the i.MX 8X EVM Kit, the Manufacturing Tool (MFGTool) is used to download and run the OS images on target devices. The MFGTool supports the serial download mode, which is a special mode that allows the tool to communicate with the device even if no OS is installed.

Regards

0 项奖励
回复

1,373 次查看
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
The Serial Downloader provides a means to download a Program Image to the chip over USB serial connection.
 
To use the serial download mode, one needs to set boot mode pins accordingly. Please refer to Table 5-1. Boot MODE Pin Settings from the Reference Manual IMX8DQXPRM.
 

To know more about serial download boot, please refer to section 5.10 Serial Downloader Boot from the Reference Manual IMX8DQXPRM.

Please refer to this document for MFG Tools.
 
Thanks & Regards

Sanket Parekh

0 项奖励
回复