manufacturing tool question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

manufacturing tool question

1,424件の閲覧回数
sivaci2754
Contributor I

For i.MX 8X EVM Kit usage, Could you please let us know how to use the serial download mode for the Manufacturing tool? It seems to be not enough to understand the procedure of usage.

What kind of tools can be supported in the serial boot mode?  https://tutuappx.com/ Vidmate

0 件の賞賛
返信
2 返答(返信)

1,404件の閲覧回数
ramprakash08
Contributor IV

Hi,

For the i.MX 8X EVM Kit, the Manufacturing Tool (MFGTool) is used to download and run the OS images on target devices. The MFGTool supports the serial download mode, which is a special mode that allows the tool to communicate with the device even if no OS is installed.

Regards

0 件の賞賛
返信

1,379件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
The Serial Downloader provides a means to download a Program Image to the chip over USB serial connection.
 
To use the serial download mode, one needs to set boot mode pins accordingly. Please refer to Table 5-1. Boot MODE Pin Settings from the Reference Manual IMX8DQXPRM.
 

To know more about serial download boot, please refer to section 5.10 Serial Downloader Boot from the Reference Manual IMX8DQXPRM.

Please refer to this document for MFG Tools.
 
Thanks & Regards

Sanket Parekh

0 件の賞賛
返信