manufacturing tool question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

manufacturing tool question

1,427 Views
sivaci2754
Contributor I

For i.MX 8X EVM Kit usage, Could you please let us know how to use the serial download mode for the Manufacturing tool? It seems to be not enough to understand the procedure of usage.

What kind of tools can be supported in the serial boot mode?  https://tutuappx.com/ Vidmate

0 Kudos
Reply
2 Replies

1,407 Views
ramprakash08
Contributor IV

Hi,

For the i.MX 8X EVM Kit, the Manufacturing Tool (MFGTool) is used to download and run the OS images on target devices. The MFGTool supports the serial download mode, which is a special mode that allows the tool to communicate with the device even if no OS is installed.

Regards

0 Kudos
Reply

1,382 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport
 
I hope you are doing well
 
The Serial Downloader provides a means to download a Program Image to the chip over USB serial connection.
 
To use the serial download mode, one needs to set boot mode pins accordingly. Please refer to Table 5-1. Boot MODE Pin Settings from the Reference Manual IMX8DQXPRM.
 

To know more about serial download boot, please refer to section 5.10 Serial Downloader Boot from the Reference Manual IMX8DQXPRM.

Please refer to this document for MFG Tools.
 
Thanks & Regards

Sanket Parekh

0 Kudos
Reply