manifest default.xml not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

manifest default.xml not found

6,729 Views
navin
Contributor I

Hi there,

I've faced an issue during creating yocto project. when i try to create project  i have got this error "manifest default.xml not found"

There are some details below.No LSB modules are available.
Distributor ID: Ubuntu
Description: Ubuntu 22.04.3 LTS
Release: 22.04
Codename: jammy

 

$ sudo apt install gawk wget git diffstat unzip texinfo gcc build-essential \
chrpath socat cpio python3 python3-pip python3-pexpect xz-utils debianutils \
iputils-ping python3-git python3-jinja2 libegl1-mesa libsdl1.2-dev \
python3-subunit mesa-common-dev zstd liblz4-tool file locales -y
$ sudo locale-gen en_US.UTF-8

mkdir ~/bin (this step may not be needed if the bin folder already exists)
$ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo

 

export PATH=~/bin:$PATH

 

$ mkdir imx-yocto-bsp
$ cd imx-yocto-bsp
$ repo init -u https://github.com/nxp-imx/imx-manifest
-b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml

repo: reusing existing repo client checkout in /home/smartbuild
fatal: manifest 'default.xml' not available
fatal: manifest default.xml not found
================================================================================
Repo command failed: UpdateManifestError
-b: command not found

 

 

0 Kudos
Reply
1 Reply

6,698 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

It seems that you are not specifying the -b command on the same line, it should be:

repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-mickledore -m imx-6.1.36-2.1.0.xml

Best regards.

0 Kudos
Reply