main differences between Linux and winCE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

main differences between Linux and winCE

2,274件の閲覧回数
mv_shishkov
Contributor II

Could you tell me all main differences (licence, easy interchanging with processors, etc.) between Linux and winCE?

3 返答(返信)

2,147件の閲覧回数
mv_shishkov
Contributor II

thank you very much

0 件の賞賛
返信

2,147件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

There are many differences  between both Operating Systems since always have been consider the opositive one from another, let try to  give you a comparation :

WINCE
Linux
All distributions has a cost in their LicenseAll distributions are for FREE
MIcrosoft Support Direct under some CostCommunity Support by FREE
Interchangeability only for Support Processors from MicrosoftBasically all Architecture of Processors are Supported and easy to build with MAKE file Cross Compiling supported
Multimedia Packages under DirectXA lot of different option of Frameworks, freescale use GSTREAMER
Codecs need to be compatible with DirectXCODEC support by the Framework.
Drivers review and approved by Microsoft less possible of bug since more deep testingDrivers provided by the Linux Community many people testing and contributing not an allign testing official process.

Let me know if you have another question


Have a great day,
Jaime

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,147件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Maksim,

You can go to google search for help:smileyhappy:~~
Have a great day,

Best Regards

Dan

0 件の賞賛
返信