m4fwloader issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

m4fwloader issues

1,932件の閲覧回数
suryapradhan
Contributor II

Hello 

I am  working with  IMX7D based board & using "m4fwloader" tool to load,start & stop the firmware to Cortex-M4 from linux- cortex A7.

But i got one issue here, while stopping the firmware & starting again.

Scenario:

I am using "rpmsg_str_echo_freertos_example.bin" firmware & able to communicate with M4 properly.

Next i  stopped it & started it again using "m4fwloader stop" & "m4fwloader start" command.

Now if i do  "echo hi > /dev/ttyRPMSG", i am getting all my previous messages[message from last communication] along with new message.

 

Any suggestion on this.

 

Regards

Surya

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,672件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Surya

what bsp used in the case, had you tried with official nxp releases described on

i.MX Software|NXP 

using nxp i.MX7 Sabre SD reference board.

Seems it can be debugged using sources info given in

New i.MX6SX & i.MX7D AMP debugging tool: imx-m4fwloader 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信