i.MX6SoloX and i.MX7D SoC contain embedded Cortex-M4 core. In a common use-case, this core runs a firmware loaded by u-boot bootloader. If you however want to debug your application for the Cortex-M4 core, you may need to reload the firmware in the secondary core without restarting Linux running on the Cortex-A core. For this reason, a tool was created: imx-m4fwloader.
The project is released as open source under GPL-2.0 licence here: GitHub - NXPmicro/imx-m4fwloader: Tool for loading firmware to M4 core on i.MX6SX and 7D
I hope this tool will help to bring up faster your application for i.MX6SoloX and i.MX7D SoC!
source /opt/poky/1.8/environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi$CC m4fwloader.c -o m4fwloader./m4fwloader myapp.bin 0x00910000./m4fwloader kick 0m4fwloader [filename.bin] [0xLOADADDR] [--verbose] # loads new firmwarem4fwloader stop # holds the auxiliary core in resetm4fwloader start # releases the auxiliary core from resetm4fwloader kick [n] # triggers interrupt on RPMsg virtqueue nI can't get this utility to work on an i.mx7. Could you help me out? I've started a forum post here: https://community.nxp.com/message/936211
This is maybe an obvious question, but could you confirm that this tool runs on Linux on Cortex A core?
I've forked out from original, and did bug fixes to it. (It really wouldn't work at all without it. )
Find fork here: GitHub - dry-75/imx-m4fwloader: Tool for loading firmware to M4 core on i.MX6SX and 7D
Tested on what I work with now - iMX7D. OCRAM and TCM memory.
Thank you for the tool.
Try the fork with fixes. Works for me on IMX7D,A7,Linux.
Updated by branch as per iMX7 DRM 2018 update and omissions, as per discussion here (and my support request ticket ..)