lwip stack ping command

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lwip stack ping command

1,868 Views
sandeep_c
Contributor I

hi im developing the driver for ksz8851snli, as of now i need to ping between the microcontroller to the pc and vice versa.

as per the icmp protocol when hit an ping command in cmd terminal iam getting 66bytes of data but as per the standard i have to get 64bytes of data, iam not getting 2 bytes extra why? i gone through the datasheet but i didnt get why iam getting 2 bytes extra,

https://ww1.microchip.com/downloads/en/DeviceDoc/KSZ8851SNL-Single-Port-Ethernet-Controller-with-SPI...

 

while iam pinging from mc to pc the mac address1st byte of data is missing this is i observed in wireshark 

 what are the analyzers i can use to debug the ethernet protocol 

 

0 Kudos
Reply
2 Replies

1,842 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hi @sandeep_c 

I hope you are doing well.
 
Please mention the processor part number.
 
Thanks & Regards,
Sanket Parekh
0 Kudos
Reply

1,835 Views
sandeep_c
Contributor I
i.MX RT1170
0 Kudos
Reply