ltib "mfg firmware profile" build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib "mfg firmware profile" build error

1,248 Views
sangjinhong
Contributor III

ltib "min profile" build ssuccessful.

However, "mfg firmware profile" failed.

The following is error message.

Could anybody let know why???

=================== error message =================

+ [ /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 != /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 ]

+ cd /home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08

+ [ -n  ]

+ make HOSTCC=ccache /usr/bin/gcc -B/usr/bin/ CROSS_COMPILE=arm-none-linux-gnueabi- O=/home/john/dev/freescale/dev_env/ltib/rpm/BUILD/u-boot-2009.08 mx6dl_sabresd_mfg_config

make: *** No rule to make target `mx6dl_sabresd_mfg_config'.  Stop.

error: Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)

RPM build errors:

    Bad exit status from /home/john/dev/freescale/dev_env/ltib/tmp/rpm-tmp.23807 (%build)

Build time for u-boot-v2009.08: 0 seconds

Failed building u-boot-v2009.08

f_buildrpms() returned an error, exiting

traceback:

main:572

Started: Wed Feb  5 15:09:11 2014

Ended:   Wed Feb  5 15:09:14 2014

Elapsed: 3 seconds

These packages failed to build:

u-boot-v2009.08

Build Failed

Exiting on error or interrupt

Labels (1)
0 Kudos
Reply
1 Reply

1,103 Views
sangjinhong
Contributor III

There are my mistakes.

0 Kudos
Reply