ltib problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib problem

977 Views
leeallen
Contributor I

when I install ltib,I meet some problem

allen@ubuntu:~/imx6/L3.0.35_4.1.0_130816_source/ltib_install/ltib$ ./ltib

Installing host support packages.

This only needs to be done once per host, but may take up to
an hour to complete ...

If an error occurs, a log file with the full output may be found in:
/home/allen/imx6/L3.0.35_4.1.0_130816_source/ltib_install/ltib/host_config.log

Exiting on error or interrupt
Please see >> /home/allen/imx6/L3.0.35_4.1.0_130816_source/ltib_install/ltib/host_config.log for details

so,I open up the file named host_config.log .

Updating lpp from local packages
+ cp -dp /home/allen/imx6/L3.0.35_4.1.0_130816_source/ltib_install/ltib/pkgs/LTIB Codecs /opt/freescale/pkgs/LTIB Codecs
cp: target `Codecs' is not a directory
Died at ./ltib line 2518.
traceback:
main::check_dirs:2518
  main::host_checks:1438
   main:554

Started: Tue Sep  8 00:27:17 2015
Ended:   Tue Sep  8 00:27:19 2015
Elapsed: 2 seconds

Build Failed

I dont know how to solve this error . may someone give me some advice?  thx ! 

Labels (1)
0 Kudos
Reply
0 Replies