ltib libi2c missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib libi2c missing

Jump to solution
5,368 Views
katte
Contributor II

Hi, I'm trying to use i2ctools on imx28evk board for communicate with an external eeprom.

My eeprom is probed by the system.

My problem is that the commands i2cdetect, i2cget... gives me this output:

i2cdetect: error while loading shared libraries: libi2c.so.0: cannot open shared object file: No such file or directory

I've tried on 2.6.35_1.1.0_130130 BSP and also on 2.6.35_10.12.

Any help will be appreciated

Labels (3)
Tags (3)
1 Solution
4,180 Views
igorpadykov
NXP Employee
NXP Employee

HI Marco

one can look at i2c-tools solution at

i2c-test tools issue in I.MX28 BSP on I.MX28 EVK

i2c-tools - Hack to program EEPROM I2C devices for MX28 boot 

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
4,181 Views
igorpadykov
NXP Employee
NXP Employee

HI Marco

one can look at i2c-tools solution at

i2c-test tools issue in I.MX28 BSP on I.MX28 EVK

i2c-tools - Hack to program EEPROM I2C devices for MX28 boot 

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------