ltib cross compiler libxv-dev progra

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ltib cross compiler libxv-dev progra

4,019件の閲覧回数
cachegxp
Contributor I

I need to use ltib cross compiler, the # include <X11/extensions/Xvlib.h> This requires the use libxv-dev, but use Ltib compiled system, the library, how to do?...

ラベル(1)
タグ(2)
0 件の賞賛
返信
8 返答(返信)

3,854件の閲覧回数
cachegxp
Contributor I

302-x11.JPGsudo find /-name Xvlib.h not find Xvlib.h file.

Xvlib.h is needed.

0 件の賞賛
返信

3,854件の閲覧回数
KrishnaPavan
Contributor II

Do one thing run

sudo find / -name Xvlib.h

and see if it's available.

By the Way, what is the software package that requires Xvlib.h?

0 件の賞賛
返信

3,854件の閲覧回数
cachegxp
Contributor I

304-x11.JPG

libXext is there, but to no avail, I would like to need libXv, but no ltib...

0 件の賞賛
返信

3,854件の閲覧回数
KrishnaPavan
Contributor II

Hi cache gxp,

In configuration, go for X11 build options and check libXext.

Regards :: Krishna Pavan

0 件の賞賛
返信

3,854件の閲覧回数
cachegxp
Contributor I

 how installed Xext?

0 件の賞賛
返信

3,854件の閲覧回数
KrishnaPavan
Contributor II

Hi,

Have you installed Xext?

If you even have sdl cross_compiled and installed, you will have that file.

What I don't understand is, whether you need that header file / library / what?

Regards :: KRISHNA PAVAN

0 件の賞賛
返信

3,854件の閲覧回数
cachegxp
Contributor I
X11 in the LTIB configuration not libxv
0 件の賞賛
返信

3,854件の閲覧回数
KrishnaPavan
Contributor II

Hi,

Have you checked for X11 in the LTIB configuration!

Regards :: Krishna Pavan

0 件の賞賛
返信