ltib build failed imx53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib build failed imx53

1,557 Views
Hitex
Contributor I

Screenshot-1.pngIfx%20Getting%20Started%20iMX53%20-%20Installing%20Inflexion%20UI%20on%20Linux.pdf

Processing: gst-plugins-ugly
==============================

Processing: gst-ffmpeg
========================
Build path taken because: no prebuilt rpm,
Testing network connectivity
No network download connection available

WARN: skipping md5sum check for /opt/freescale/pkgs/gst-ffmpeg-0.10.3.tar.bz2, md5 file was not found
Can't get: gst-ffmpeg-0.10.3-relink.patch at ./ltib line 790.


f_buildrpms() returned an error, exiting
traceback:
 main:560


Started: Fri Jan 20 03:47:40 2012
Ended:   Fri Jan 20 03:48:17 2012
Elapsed: 37 seconds

These packages failed to build:
gst-ffmpeg

Build Failed

I am following the steps given in the pdf. However I am getting the following error. I attached the screen shot of the error and the pdf.

Thanks

Hitesh

Tags (1)
0 Kudos
Reply
3 Replies

1,355 Views
Hitex
Contributor I

hi i resolved the issue. i downloaded the relink patch and put in the respective folder still i got error telling relink patch is a garbage file so i downloaded gst-ffmpeg-0.10.3.tar.bz2.md5 and put it in the same folder.

0 Kudos
Reply

1,355 Views
Hitex
Contributor I

Thanks Vladan

i have set http_proxy and I am able to install packages using "apt-get install" so do u still think its a network issue.

Regards

Hitesh

0 Kudos
Reply

1,355 Views
VladanJovanovic
NXP Employee
NXP Employee

LTIB is trying to get a package via network and it seems you have no network available for downloading the package...

0 Kudos
Reply