ltib build error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ltib build error

9,474 次查看
MuhammadOmarFar
Contributor I

Hey,

I am performing ltib build operation as shown in  the step 4 in section 2.2 in the document that i have attached.

but this error is coming

"ltib can not run because one or more host packages needed to run it are either missing or out of date or not in ltib's standard path" .

 i am a newbie :( ..can any one help me ?

标签 (1)
0 项奖励
回复
2 回复数

9,308 次查看
RandyKrakora
NXP Employee
NXP Employee

Here's some info here:

http://www.imxdev.org/wiki/index.php?title=ALL_Boards_ltib_config_ubuntu

Make a mental note of this step though -> "Ubuntu distro uses dash instead of bash as shell, then change it to bash:", it probably won't hurt you, but there are some differences in scripting across the two shells.

But either way, I followed the instructions exactly, then ltib worked fine.

-Randy

0 项奖励
回复

9,308 次查看
KrishnaPavan
Contributor II

look in the error log!

0 项奖励
回复