ltib build error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib build error

9,489 Views
MuhammadOmarFar
Contributor I

Hey,

I am performing ltib build operation as shown in  the step 4 in section 2.2 in the document that i have attached.

but this error is coming

"ltib can not run because one or more host packages needed to run it are either missing or out of date or not in ltib's standard path" .

 i am a newbie :( ..can any one help me ?

Labels (1)
0 Kudos
Reply
2 Replies

9,323 Views
RandyKrakora
NXP Employee
NXP Employee

Here's some info here:

http://www.imxdev.org/wiki/index.php?title=ALL_Boards_ltib_config_ubuntu

Make a mental note of this step though -> "Ubuntu distro uses dash instead of bash as shell, then change it to bash:", it probably won't hurt you, but there are some differences in scripting across the two shells.

But either way, I followed the instructions exactly, then ltib worked fine.

-Randy

0 Kudos
Reply

9,323 Views
KrishnaPavan
Contributor II

look in the error log!

0 Kudos
Reply