ltib and fsl-mm-codeclib configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ltib and fsl-mm-codeclib configuration

Jump to solution
2,561 Views
machlee
Contributor II

Dear All,

I have got a problem while setup ltib like below.

I'm trying with I.MX53 QSB (aka loco).

Please help me if any hints...

....................

Processing: fsl-mm-codeclib

=============================

Build path taken because: no prebuilt rpm,

Testing network connectivity

OK GPP:

Try fsl-mm-codeclib-2.0.3.tar.gz.md5 from the GPP

http://bitshrine.org/gpp/fsl-mm-codeclib-2.0.3.tar.gz.md5:

23:01:09 ERROR 404: Not Found.

Try fsl-mm-codeclib-2.0.3.tar.gz from the GPP

http://bitshrine.org/gpp/fsl-mm-codeclib-2.0.3.tar.gz:

23:01:10 ERROR 404: Not Found.

Can't get: fsl-mm-codeclib-2.0.3.tar.gz at ./ltib line 790.

f_buildrpms() returned an error, exiting

traceback:

main:560

Labels (4)
0 Kudos
Reply
1 Solution
1,877 Views
RodBorras
NXP Employee
NXP Employee

Hi,

Two things need to happen for a package to build:

  a) the package tar,gz name is defined in ltib/dist/lfs-5.1/<package>/<package>.spec

  b) the package tar.gz from a) must be found with the exact same spelling in /opt/freescale/pkgs

Did you download IMX_MMCODECS_11.09.tar.gz?

You have to download the above, untar it, and copy all the files in IMX_MMCODECS_11.09/Ltib Files/ to /opt/freescale/pkgs  (you will find the missing fsl-mm-codeclib-2.0.3.tar.gz and fsl-mm-codeclib-2.0.3.tar.gz.md5 in that Ltib files folder).

Hope this works for you,

Rod.

View solution in original post

0 Kudos
Reply
2 Replies
1,877 Views
machlee
Contributor II

Dear Rod,

Thank you for your help.

I have cleared with your hints.

There was a fsl-mm/ directory under ltib/dist/lfs-5.1/ and

I just copied all the files in IMX_MMCODECS_11.09/Ltib Files/ to /opt/freescale/pkgs.

And It worked fine.

Thanks a lot.

Mach

0 Kudos
Reply
1,878 Views
RodBorras
NXP Employee
NXP Employee

Hi,

Two things need to happen for a package to build:

  a) the package tar,gz name is defined in ltib/dist/lfs-5.1/<package>/<package>.spec

  b) the package tar.gz from a) must be found with the exact same spelling in /opt/freescale/pkgs

Did you download IMX_MMCODECS_11.09.tar.gz?

You have to download the above, untar it, and copy all the files in IMX_MMCODECS_11.09/Ltib Files/ to /opt/freescale/pkgs  (you will find the missing fsl-mm-codeclib-2.0.3.tar.gz and fsl-mm-codeclib-2.0.3.tar.gz.md5 in that Ltib files folder).

Hope this works for you,

Rod.

0 Kudos
Reply