loading the os image into sd card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

loading the os image into sd card

跳至解决方案
1,970 次查看
shankovai
Contributor III

Hello support team,

Configuration

Build Configuration:
BB_VERSION = "2.0.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "universal"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6qdlsabresd"
DISTRO = "fsl-imx-wayland"
DISTRO_VERSION = "5.15-kirkstone"
TUNE_FEATURES = "arm vfp cortexa9 neon thumb callconvention-hard"
TARGET_FPU = "hard"
meta
meta-poky = "HEAD:27de52e402ae000dfa502d52908cd6e6aef923ec"
meta-oe
meta-multimedia
meta-python = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-freescale = "HEAD:2fb1ce365338126aad365012ebb913b3e4a9f1be"
meta-freescale-3rdparty = "HEAD:de0eb1408150d77f9cce97c559f9a5a3c71e5d6c"
meta-freescale-distro = "HEAD:fc15f5003043da23212596be7366ae2547c308ad"
meta-bsp
meta-sdk
meta-ml
meta-v2x = "HEAD:5bc708f56575a878da17f2148e959c95d06cf8db"
meta-nxp-demo-experience = "HEAD:8fade3993b832ecd823771644f2a7b731f8f4527"
meta-chromium = "HEAD:d25d8ee98a656b2534d0eec6138ef264529fab4f"
meta-clang = "HEAD:85d956d95401479ca666139e31f662f60c156d5f"
meta-gnome
meta-networking
meta-filesystems = "HEAD:5357c7a40eaf8d1bcf7ff58edbba8e9527e40c7d"
meta-qt6 = "HEAD:b2894aad5c1aaa85f2f5c7b94391b7c51c39e555"
meta-virtualization = "HEAD:973c8d0964c6f40338857efe5b8009b2f647d485"

bitbake core-image-minimal

after building the image, flash the image into sd card by giving below command

bzcat <image_name>.wic.bz2 | sudo dd of=/dev/sd<partition> bs=1M conv=fsync

 

sudo fdisk /dev/sda  -l
Disk /dev/sda: 29.3 GiB, 31457280000 bytes, 61440000 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0x3f9d3c50

Device     Boot Start    End Sectors   Size Id Type
/dev/sda1  *     8192  60825   52634  25.7M  c W95 FAT32 (LBA)
/dev/sda2       65536 288921  223386 109.1M 83 Linux

question

usually three partition will be generated ? but  from the above two partition are shown, is the above is correct

uboot.sb will be burned in partition1 (memory loader FSBL)

uimage and .dtb burned in partition2 (Uboot, environment variable)

rootfs,linux image(dev,etc......) burned in partition3 (rootfs, uimage)

 

please confirm

0 项奖励
回复
1 解答
1,961 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @shankovai 

Two partitions are correct. U-boot, dtb, and kernel will be stored at first partition. Rootfs will be at second partition.

Best regards

Harvey

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,962 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @shankovai 

Two partitions are correct. U-boot, dtb, and kernel will be stored at first partition. Rootfs will be at second partition.

Best regards

Harvey

0 项奖励
回复