load sdma firmware without udev

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

load sdma firmware without udev

4,184 Views
jerry_zeng
Contributor I

My project uses iMX6 with Linux 4.14.126 by Timesys, but we need to disable udev. How can the sdma-imx6q.bin firmware be loaded from user space without udev? One more question: can the sdma-imx6q.bin firmware be built into Linux kernel image from its source code? if can, please let me know in details.

Thanks,

Jerry

0 Kudos
Reply
4 Replies

3,940 Views
jerry_zeng
Contributor I

Hi Igor,

Thank you very much for the quick response. My original general question is how to load iMX6 sdma firmware (sdma-imx6q.bin) from user space without UDEV enabled, and it has nothing to do with Timesys. Can you please specify it?

Thanks,

Jerry

0 Kudos
Reply

3,940 Views
ceggers1
Contributor IV

Hi Jerry,

modern Linux kernels do not need udev at all for firmware loading. All required functionality is built into the kernel, so no userspace tools are required anymore.

You only have to specify the filename of the SDMA firmware in the device tree node of the SDMA. The firmware file then needs to be placed under /lib/firmware/.

You have to take care, that the firmware is available when the SDMA driver is initialized. I'm not sure what happens if the SDMA driver is linked into the kernel (no module). Maybe the initialization happens before the root fs is mounted and the firmware is not available yet. In my project, I have compiled the SDMA driver as a kernel module which is loaded after the root fs is available.

Technically you could link the SDMA firmware binary into the kernel (as builtin firmware). But in my opinion the license of the SDMA firmware is incompatible to the GPLv2 of the kernel.

I hope that I could answer you questions. If you have further questions about the SDMA, don't hesitate to contact me directly (I don't read the forum every day).

Best regards

Christian

0 Kudos
Reply

3,940 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jerry

may be useful to check Freescale i.MX SDMA tutorial (part I) 

There are no special actions for loading sdma firmware, nxp

linux is performing this automatically. One can try nxp linux from

source.codeaurora.org/external/imx/linux-imx  repository
linux-imx - i.MX Linux kernel 

Best regards
igor

0 Kudos
Reply

3,940 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jerry

sdma is proprietary nxp software its sources are not available for customers.

Regarding timesys linux, it is supported directly by timesys support, issue

may be posted on

TimeSys Linux GPL | Support for TimeSys Linux GPL at SourceForge.net 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply