linux logo in MIPI DSI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux logo in MIPI DSI

3,407件の閲覧回数
jigneshpatel
Contributor III

I am working on i. MX6 Dualite Processors with linux kernel revision 4.9.88 and Debian file system.

I have interfaced MIPI display.
It directly display xorg screen, linux logo is not displaying.

BSP has a default LVDS interface and changes to MIPI. in LVDS it displays linux logo properly.

Please help me to solve issue of linux logo.

Thanks in advance.

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

2,994件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jignesh

one can try to use patch below

Patch to support MIPI display(hx8369) in uboot for i.mx6DL/DQ SebreSD boards 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,994件の閲覧回数
jigneshpatel
Contributor III

Thanks igor,

For uboot,

I will check uboot patch.

Now my uboot argument is: "setenv videoargs bootargs ${bootargs} video=mxcfb0:dev=mipi_dsi,TRULY-WVGA,if=RGB24;"

For kernel,

My mipi driver is probing perfect because xorg is displayed perfect.
For Displaying logo, I have print debug to verfiy the logo display function.

  fbmem.c DEBUG  line = 618 fb_prepare_logo : fb_prepare_logo
  fbmem.c DEBUG  line = 638 fb_prepare_logo : found suitable logo
  fbmem.c DEBUG  line = 652 fb_prepare_logo : logo xres 480 and yres 800
  fbmem.c DEBUG  line = 663 fb_prepare_logo : 24 bit logo depth
Console: switching to colour frame buffer device 60x50
  fbmem.c DEBUG  line = 700 fb_show_logo : fb_show_logo
  fbmem.c DEBUG  line = 487 fb_show_logo_line : fb_show_logo_line
  fbmem.c DEBUG  line = 250 fb_set_logo_truepalette : fb_set_logo_truepalette
  fbmem.c DEBUG  line = 442 fb_do_show_logo : fb_do_show_logo
  fbmem.c DEBUG  line = 705 fb_show_logo : Logo displayed 80

Above all debug print after MIPI DSI panel initialization.

Please guide me for follwing queries
1. Why my linux logo is not printed?
2. Is uboot patch(MIPI-DSI) is required to display linux kernel logo?

Thanks,
Jignesh Patel

0 件の賞賛
返信

2,994件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jignesh

nxp does not support debian, please try linux from nxp official repository

linux-imx - i.MX Linux kernel 

Best regards
igor

0 件の賞賛
返信