linux crashing in reset_ctrl_regs in hw_breakpoints.c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linux crashing in reset_ctrl_regs in hw_breakpoints.c

1,851 Views
dennish
Contributor I

Linux is crashing with an invalid instruction in arch/arm/kernel/hw_breakpoiint.c (reset_crtl_regs) for an i.MX6 solo.

I see calls to smp_processor_id() and several assembly mcr/mrc instruction to the breakpoint coprocessor.

Has anyone seen something similar?

Thank you

Dennis

Labels (2)
0 Kudos
Reply
4 Replies

1,715 Views
jimmychan
NXP TechSupport
NXP TechSupport

what BSP and which board are you using?


0 Kudos
Reply

1,715 Views
dennish
Contributor I

Hi Jimmy.

I'm using Freescale's L3.0.35_3.0.0_121207 SDL bsp.

I have also installed the 3.0.1 and 3.0.3 patches.

Thank you,

Dennis

0 Kudos
Reply

1,715 Views
Ragan_Dunham
NXP Employee
NXP Employee

We've not seen this before.  Which board are you using?  And can you describe what is happening in the system when the crash occurs?  Are you booting or running a specific app or do it just occur randomly or ...?  Thanks for any additional details you are able to provide.

Regards,

Ragan

0 Kudos
Reply

1,715 Views
admin
Specialist II

Dennis, any more input?

0 Kudos
Reply