linux-can has moved from gitorious.org to github.com

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linux-can has moved from gitorious.org to github.com

1,506 次查看
fweller
Senior Contributor I

The linux-can project has moved from gitorious.org to github.com

This has not been updated in the yocto bitbake recipe for the previous generation fsl-release-bsp-3.10.17_1.0.0

I ran in to this issue while compiling the Freescale Linux release 3.10.17 for the SABRE Smart Devices Platform MCIMX6Q-SDP

This HAS been corrected in the latest Freescale release 3.10.53

The bitbake error looks like this:

ERROR: Function failed: Fetcher failure for URL: 'git://git.gitorious.org/linux-can/can-utils.git;protocol=git'. Unable to fetch URL from any source.

ERROR: Logfile of failure stored in: ....../fsl-release-bsp-3.10.17_1.0.0/build/tmp/work/cortexa9hf-vfp-neon-poky-linux-gnueabi/can-utils/1.0-r0/temp/log.do_fetch.93285

ERROR: Task 1935 (....../fsl-release-bsp-3.10.17_1.0.0/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-connectivity/can-utils/can-utils_1.0.bb, do_fetch) failed with exit code '1'

The correction I made was to edit the file .../fsl-release-bsp-3.10.17_1.0.0/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-connectivity/can-utils/can-utils_1.0.bb

Change line 11:

FROM:   SRC_URI = "git://git.gitorious.org/linux-can/${BPN}.git;protocol=git;branch=master"

TO:   SRC_URI = "git://github.com/linux-can/${BPN}.git;protocol=git;branch=master"

标签 (2)
标记 (3)
0 项奖励
回复
1 回复

1,017 次查看
fabio_estevam
NXP Employee
NXP Employee

Flint,

Care to submit a patch to meta-fsl-arm list?

Thanks,

Fabio Estevam

0 项奖励
回复