linux camera failed in long time recording

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

linux camera failed in long time recording

1,156 次查看
kevin_chan
Contributor III

platform: imx6q sabresd evk board

software: L3.0.35_4.1.0

i use gst to record from mipi camera (0v5640):

gst-launch mfw_v4lsrc fps-n=30 capture-mode=0 device=/dev/video1 ! queue ! vpuenc codec=6 ! matroskamux ! filesink location=mipi.mkv sync=false &

gst start record, but after some time, about 15 minutes, gst aborted with these error log: /****************************************************************************************************

ERROR: from element /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0: Internal data flow error.                                                                  

Additional debug info:

gstbasesrc.c(2582): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0:

streaming task paused, reason error (-5)

Execution ended after 31058324004 ns.

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

Setting pipeline to NULL ...

Freeing pipeline ...

[1]+  Done                      gst-launch mfw_v4lsrc fps-n=30 capture-mode=0 device=/dev/video1 ! queue ! vpuenc codec=6 ! matroskamux ! filesink location=mipi.mkv sync=false

/****************************************************************************************************

i try to see the size of ouput:

du -sh mipi.mkv  ----------  40.0M  mipi.mkv

And  yocto-3.10.17_1.0.0 bsp  has this problem too.

And a step further,  i test this command:

gst-launch mfw_v4lsrc fps-n=30 capture-mode=0 device=/dev/video1 ! queue ! vpuenc codec=6 ! matroskamux ! fakesink sync=false &

it's ok even after 30 minutes.

can someone give me suggestion about this gst problem?

we need to do a long time camera recording. thanks

标签 (3)
标记 (2)
0 项奖励
回复
1 回复

986 次查看
Yuri
NXP Employee
NXP Employee

  Please try using queue-size option of mfw_v4lsrc element.

$ gst-launch mfw_v4lsrc fps-n=30 capture-mode=0 device=/dev/video1  queue-size= 10 ! queue ! vpuenc codec=6 ! matroskamux ! filesink location=mipi.mkv sync=false


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复