line 757: uuu: command not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

line 757: uuu: command not found

跳至解决方案
5,009 次查看
chatchai
Contributor I

I try to use UUU downloaded from Github for Linux.  error at line 757: uuu: command not found


my terminal

bsp@bsp-desktop:~/Downloads/android-10.0.0_2.3.0_image_8mmevk$ sudo ~/Downloads/android-10.0.0_2.3.0_image_8mmevk/uuu_imx_android_flash.sh -f imx8mm -a -e -u trusty
[sudo] password for bsp:
This script is validated with uuu 1.3.124 version, it is recommended to align with this version.
dtbo is supported
dual slot is supported
dynamic parttition is supported
generate lines to flash u-boot-imx8mm-trusty.imx to the partition of bootloader0
generate lines to flash partition-table.img to the partition of gpt
generate lines to flash dtbo-imx8mm.img to the partition of dtbo_a
generate lines to flash boot.img to the partition of boot_a
generate lines to flash vbmeta-imx8mm.img to the partition of vbmeta_a
lpmake I 09-10 10:02:58 119432 119432 builder.cpp:937] [liblp]Partition system_a will resize from 0 bytes to 918253568 bytes
lpmake I 09-10 10:02:58 119432 119432 builder.cpp:937] [liblp]Partition vendor_a will resize from 0 bytes to 75804672 bytes
lpmake I 09-10 10:02:58 119432 119432 builder.cpp:937] [liblp]Partition product_a will resize from 0 bytes to 335319040 bytes
generate lines to flash super.img to the partition of super
uuu script generated, start to invoke uuu with the generated uuu script
/home/bsp/Downloads/android-10.0.0_2.3.0_image_8mmevk/uuu_imx_android_flash.sh: line 757: uuu: command not found
bsp@bsp-desktop:~/Downloads/android-10.0.0_2.3.0_image_8mmevk$

0 项奖励
回复
1 解答
4,979 次查看
chatchai
Contributor I

Thank you for your reply 

Now I just flash to my board with invoking uuu.lst in tmp folder as SUPERUSER after run uuu_imx_android_flash.sh script.

My step

$ sudo ~/<image_dir>/uuu_imx_android_flash.sh -f imx8mm -a -e -u trusty

#..........line 757: uuu: command not found (this is final command in script)

$ sudo su
$ ./uuu /tmp/uuu.lst

Now start flashing to my board and success.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
4,992 次查看
b36401
NXP Employee
NXP Employee

Please try to add the directory uuu binary is located into $PATH variable.

0 项奖励
回复
4,980 次查看
chatchai
Contributor I

Thank you for your reply 

Now I just flash to my board with invoking uuu.lst in tmp folder as SUPERUSER after run uuu_imx_android_flash.sh script.

My step

$ sudo ~/<image_dir>/uuu_imx_android_flash.sh -f imx8mm -a -e -u trusty

#..........line 757: uuu: command not found (this is final command in script)

$ sudo su
$ ./uuu /tmp/uuu.lst

Now start flashing to my board and success.

0 项奖励
回复