libmfwba.so: cannot open shared object file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

libmfwba.so: cannot open shared object file

2,192件の閲覧回数
alokkumar
Contributor III

I am getting following error when writing a sample program in C++ for qt and gsteamer on nitrogen6X (imx6Q) board. I am using timesys mid march 2013 release.

----

GLib-CRITICAL **: g_hash_table_lookup: assertion `hash_table != NULL' failed

0:00:00.000310000  1807 (UNKNOWN FORMAT) segment start=0, stop=105536, last_stop=0, duration=105568, rate=0.000000, applied_rate=0.000000, flags=0x00, time=0:00:00.000000000, accum=0:00:00.000000000 INFO                GST_INIT gst.c:613:init_pre: Initializing GStreamer Core Library version 0.10.36

(samp1:1807): GLib-CRITICAL **: g_hash_table_lookup: assertion `hash_table != NULL' failed

0:00:00.001499334  1807 (UNKNOWN FORMAT) segment start=0, stop=105536, last_stop=0, duration=105568, rate=0.000000, applied_rate=0.000000, flags=0x00, time=0:00:00.000000000, accum=0:00:00.000000000 INFO                GST_INIT gst.c:614:init_pre: Using library installed in /usr/lib

(samp1:1807): GLib-CRITICAL **: g_hash_table_lookup: assertion `hash_table != NULL' failed

0:00:00.001752667  1807 (UNKNOWN FORMAT) segment start=0, stop=105536, last_stop=0, duration=105568, rate=0.000000, applied_rate=0.000000, flags=0x00, time=0:00:00.000000000, accum=0:00:00.000000000 INFO                GST_INIT gst.c:624:init_pre: Linux nitrogen6x 3.0.35-ts-armv7l #1 SMP PREEMPT Thu Mar 7 18:19:57 EST 2013 armv7l

0:00:00.002436334  1807 default segment start=0, stop=105536, last_stop=0, duration=105568, rate=0.000000, applied_rate=0.000000, flags=0x00, time=0:00:00.000000000, accum=0:00:00.000000000 INFO                GST_INIT gstquery.c:107:_gst_query_initialize: init queries

0:00:00.006112334  1807 default segment start=0, stop=111669308552, last_stop=0, duration=8590092504, rate=0.000000, applied_rate=0.000000, flags=0x00, time=0:02:17.438954496, accum=0:00:04.294967296 ERROR          GST_MFWBUFFER gstmfwbuffer.c:69:open_allocator_dll: Can not open dll, libmfwba.so: cannot open shared object file: No such file or directory.

--------------------------code ---------------------------------------------------------------------------

#include <QtCore/QCoreApplication>

#include <gst/gst.h>

int main(int argc, char *argv[])

{

QCoreApplication a(argc, argv);

    //GMainLoop *loop;

    gst_init (NULL,NULL);

    //loop = g_main_loop_new (NULL, FALSE);

    GstElement *bin = gst_pipeline_new ("pipeline");

    g_assert(bin);

    //GstElement *testSrc = gst_element_factory_make("videotestsrc", "source");

    GstElement *source = gst_element_factory_make("filesrc", "source");

g_assert(source);

    gchar * filename = "/home/media/bbb_short_1080p.avi";

g_object_set(G_OBJECT(source), "location", filename, "typefind",true,NULL);

    GstElement *videoconvert = gst_element_factory_make ("vpudec", "videoconvert");

    GstElement *demux = gst_element_factory_make("aiurdemux", "demux");

    GstElement *videoOut = gst_element_factory_make("mfw_isink", "videosink");

g_assert(videoOut);

gst_bin_add_many(GST_BIN(bin), source,demux, videoconvert, videoOut, NULL);

gst_element_link_many(source, videoconvert, videoOut, NULL);

gst_element_set_state(GST_ELEMENT(bin), GST_STATE_PLAYING);

    a.exec();

      /* unset */

//gst_element_set_state (GST_ELEMENT (bin), GST_STATE_NULL);

//gst_object_unref (GST_OBJECT (bin)); }

~                                

While this works with gst-launch pipeline.

Any quick suggestion is highly appreciated.

Thanks

Alok

0 件の賞賛
返信
1 返信

1,704件の閲覧回数
PrabhuSundarara
NXP Employee
NXP Employee

Can you please check with the prebuilt images (rootfs) from freescale.com. Whether the same problem is reproducible?

0 件の賞賛
返信