libipu.so for i.MX.6 query

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

libipu.so for i.MX.6 query

1,814件の閲覧回数
vikaspatil
Senior Contributor I

Hi All,

Is there a libipu available for i.MX6 (solo, quad, dual lite etc) platform? Is there any way we can use it on i.MX6?

I tired compiling ipu-lib on 1.7_Dizzy branch (i.e. imx-lib-3.10.17-1.0.0) for imx6qsabresd. However in looking at source folder it seems it picked up mxc_ipu_hl_lib_dummy.c instead of mxc_ipu_hl_lib.c dues to following code in Makefile.

ifeq ($(PLATFORM), IMX6Q)

OBJS = mxc_ipu_hl_lib_dummy.o

else

OBJS = mxc_ipu_hl_lib.o mxc_ipu_lib.o

endif

Does this means it is not available for any version of i.mx6?

Regards,

Vikas

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 返信

1,590件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

HI vikash

please refer to attached Release Notes p.10,11

Table  "Known Issues and Workarounds" :

"IPU library is removed from i.MX 6."

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信