i'm trying to get yocto imeges with qt5 by this manual at master branch Getting started with Yocto on Wandboard - Wandboard Wiki and getting error
ERROR: libimxvpuapi-0.10.1-r0 do_configure: Function failed: do_configure (log file is located at /media/data/dev/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/libimxvpuapi/0.10.1-r0/temp/log.do_configure.3965)
ERROR: Logfile of failure stored in: /media/data/dev/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/libimxvpuapi/0.10.1-r0/temp/log.do_configure.3965
Log data follows:
| DEBUG: Executing python function sysroot_cleansstate
| DEBUG: Python function sysroot_cleansstate finished
| DEBUG: Executing shell function do_configure
| waf [commands] [options]
|
| Main commands (example: ./waf build -j4)
| build : executes the build
| clean : cleans the project
| configure: configures the project
| dist : makes a tarball for redistributing the sources
| distcheck: checks if the project compiles (tarball from 'dist')
| distclean: removes the build directory
| install : installs the targets on the system
| list : lists the targets to execute
| step : executes tasks in a step-by-step fashion, for debugging
| uninstall: removes the targets installed
|
| Options:
| --version show program's version number and exit
| -h, --help show this help message and exit
| -c COLORS, --color=COLORS
| whether to use colors (yes/no/auto) [default: auto]
| -j JOBS, --jobs=JOBS amount of parallel jobs (8)
| -k, --keep continue despite errors (-kk to try harder)
| -v, --verbose verbosity level -v -vv or -vvv [default: 0]
| --zones=ZONES debugging zones (task_gen, deps, tasks, etc)
| --enable-debug enable debug build [default: False]
| --enable-static build static library [default: build shared library]
| --use-fslwrapper-backend
| use the Freescale VPU wrapper (= libfslvpuwrap) backend
| instead of the vpulib (= imx-vpu) one [default: False]
|
| Configuration options:
| -o OUT, --out=OUT build dir for the project
| -t TOP, --top=TOP src dir for the project
| --check-c-compiler=CHECK_C_COMPILER
| list of C compilers to try [gcc clang icc]
|
| Build and installation options:
| -p, --progress -p: progress bar; -pp: ide output
| --targets=TARGETS task generators, e.g. "target1,target2"
|
| Step options:
| --files=FILES files to process, by regexp, e.g.
| "*/main.c,*/test/main.o"
|
| Installation and uninstallation options:
| -f, --force force file installation
| --distcheck-args=ARGS
| arguments to pass to distcheck
|
| Installation prefix:
| By default, "waf install" will put the files in "/usr/local/bin",
| "/usr/local/lib" etc. An installation prefix other than "/usr/local" can
| be given using "--prefix", for example "--prefix=$HOME"
|
| --prefix=PREFIX installation prefix [default: '/usr/local/']
| --destdir=DESTDIR installation root [default: '']
| --exec-prefix=EXEC_PREFIX
| installation prefix for binaries [PREFIX]
|
| Installation directories:
| --bindir=BINDIR user commands [EXEC_PREFIX/bin]
| --sbindir=SBINDIR system binaries [EXEC_PREFIX/sbin]
| --libexecdir=LIBEXECDIR
| program-specific binaries [EXEC_PREFIX/libexec]
| --sysconfdir=SYSCONFDIR
| host-specific configuration [PREFIX/etc]
| --sharedstatedir=SHAREDSTATEDIR
| architecture-independent variable data [PREFIX/com]
| --localstatedir=LOCALSTATEDIR
| variable data [PREFIX/var]
| --libdir=LIBDIR object code libraries [EXEC_PREFIX/lib]
| --includedir=INCLUDEDIR
| header files [PREFIX/include]
| --oldincludedir=OLDINCLUDEDIR
| header files for non-GCC compilers [/usr/include]
| --datarootdir=DATAROOTDIR
| architecture-independent data root [PREFIX/share]
| --datadir=DATADIR architecture-independent data [DATAROOTDIR]
| --infodir=INFODIR GNU "info" documentation [DATAROOTDIR/info]
| --localedir=LOCALEDIR
| locale-dependent data [DATAROOTDIR/locale]
| --mandir=MANDIR manual pages [DATAROOTDIR/man]
| --docdir=DOCDIR documentation root [DATAROOTDIR/doc/PACKAGE]
| --htmldir=HTMLDIR HTML documentation [DOCDIR]
| --dvidir=DVIDIR DVI documentation [DOCDIR]
| --pdfdir=PDFDIR PDF documentation [DOCDIR]
| --psdir=PSDIR PostScript documentation [DOCDIR]
| waf: error: no such option: --disable-static
| WARNING: exit code 2 from a shell command.
| ERROR: Function failed: do_configure (log file is located at /media/data/dev/fsl-community-bsp/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/libimxvpuapi/0.10.1-r0/temp/log.do_configure.3965)
how i can fix it?
 
					
				
		
found a solution
[PATCH] waf.bbclass: Remove --disable-static from EXTRA_OECONF