keypad port driver in optee not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

keypad port driver in optee not working

ソリューションへジャンプ
2,616件の閲覧回数
asmaa
Contributor V

Hello Everyone,

I am writing keypad driver using imx6 keypad port in optee core . The idea is whenever key is pressed on keypad module interrupt will be generated in optee keypad driver and the value of key-pressed would be send to normal world from secure world.

I have added driver at @ /optee-os/core/drivers/keypad_driver.c

I have written keypad Pseudo TA  @ /optee-os/core/arch/arm/pta/pta_keypad.c

Please find both the attachments

I am calling pseudo TA from normal world and I am not getting any output.

I have defined KPP pin definition in device tree. my question is,

Is it right to do KPP definition in device tree if I am writing driver in Optee core,as I want to make it secure?

My device tree definition for ROW 0,1,3 and COL 0,1,2,3:

imx6ul-14x14-evk.dts

pinctrl_kpp: kppgrp {
            fsl,pins = <
                MX6UL_PAD_ENET1_RX_DATA0__KPP_ROW00        0x1B010
                MX6UL_PAD_ENET1_RX_EN__KPP_ROW01        0x1B010
                MX6UL_PAD_ENET1_TX_CLK__KPP_ROW03       0x1B010
                MX6UL_PAD_ENET1_RX_DATA1__KPP_COL00        0x110B0
                MX6UL_PAD_ENET1_TX_DATA0__KPP_COL01     0x110B0
                MX6UL_PAD_ENET1_TX_EN__KPP_COL02        0x110B0
                MX6UL_PAD_ENET1_RX_ER__KPP_COL03        0x110B0
            >;
        };

&kpp {
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_kpp>;
    >;
    status = "okay";
};

Is the above declaration correct?

I have removed compatible field, as I want to use my own driver from Optee core, Is it OK to remove?

One more question is, Do I have to enable clock in my optee keypad driver?

Can somebody please have a look at driver and PTA.

Thanks & Regards,

Asma

ラベル(1)
タグ(2)
1 解決策
2,334件の閲覧回数
asmaa
Contributor V

I was able to solve it on my own.

元の投稿で解決策を見る

7 返答(返信)
2,334件の閲覧回数
asmaa
Contributor V

Gentle reminder!!!

Could someone please help

0 件の賞賛
返信
2,334件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  the issue is under discussion.

Regards,

Yuri.

0 件の賞賛
返信
2,334件の閲覧回数
asmaa
Contributor V

YuriMuhin_ng‌,

Any update on this?

Regards,

Asma

0 件の賞賛
返信
2,334件の閲覧回数
Yuri
NXP Employee
NXP Employee

Still under consideration, sorry.

~Yuri.

0 件の賞賛
返信
2,335件の閲覧回数
asmaa
Contributor V

I was able to solve it on my own.

2,334件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

" It is Ok to modify the device tree as it fits for driver, as long as the node (kpp node) is not enabled for Linux to use.

When it comes to a clock, then yes it needs to be enabled on Optee side, but most importantly it must not be disabled on Linux side. Linux will disable any clock that is defined but not used."

Regards,

Yuri.

0 件の賞賛
返信
2,334件の閲覧回数
asmaa
Contributor V

Thank you Yuri,

I am not getting interrupt... Even though I have enabled inyerrupt.

0 件の賞賛
返信