keyctl list @s doesn't show logkey

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

keyctl list @s doesn't show logkey

2,301 次查看
richc128
Contributor III

when I boot into initramfs and then import my caam key I don't see the logon:logkey in the keyring

sh-5.1# keyctl list @s
1 key in keyring:
1028402199: --alswrv 0 65534 keyring: _uid.0

but when I boot into the regular filesystem I see it

hostname:~$ keyctl list @s
2 keys in keyring:
239354824: ----s-rv 0 0 user: invocation_id
676824911: --alsw-v 0 0 logon: logkey:

 

The only thing I can figure is there is something in the kernel  have as a module that isn't loaded with the initramfs image. What would cause this?

0 项奖励
回复
3 回复数

2,283 次查看
richc128
Contributor III
0 项奖励
回复

2,283 次查看
richc128
Contributor III

I have had success using @u instead of @s but I don't understand why.

0 项奖励
回复

2,288 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

To which board is this? and which BSP are you using?

Regards

0 项奖励
回复