kernel panic i.mx25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kernel panic i.mx25

4,751件の閲覧回数
albert_arquer
Contributor I

Hello, I have a board that is allmost identicall from the i.MX25 PDK. The problem is that every once on a while i get a kernel panic error.... I really don't know what is causing it and I don't know how to go about finding out the reason.... I don't know if hardware issues should be rulled out since the board is working most of the time or what... I mean the SDRAM and the NFC are not exactlly the same... could it be a matter of timings... I have tried flashing the kernel/bootloader/rootfs originally generated by LTIB (without performing any modification whatsoever) and it still happens....

 

Here I am copying the error output:

 

Starting the hotplug events dispatcher udevd

Synthesizing initial hotplug events

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = c3bac000

[00000000] *pgd=83ba6031, *pte=00000000, *ppte=00000000

Internal error: Oops: 817 [#1] PREEMPT

Modules linked in:

CPU: 0    Not tainted  (2.6.31-207-g7286c01 #1)

PC is at file_free_rcu+0x1c/0x64

LR is at __rcu_process_callbacks+0x224/0x2b4

pc : [<c00b6f98>]    lr : [<c0076120>]    psr: 60000013

sp : c3b7ff48  ip : 20000093  fp : 0000000a

r10: 00000020  r9 : 00000008  r8 : c042169c

r7 : 00000001  r6 : 00000002  r5 : c38e4ce0  r4 : c3898540

r3 : 00000000  r2 : c380bd28  r1 : c0419900  r0 : c38852a0

Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment user

Control: 0005317f  Table: 83bac000  DAC: 00000015

Process path_id (pid: 998, stack limit = 0xc3b7e270)

Stack: (0xc3b7ff48 to 0xc3b80000)

ff40:                   c040048c c0076120 00000036 c3b7e000 00000102 c00761c4

ff60: 00000081 c004a6a0 c3b7e000 c03fbf7c c3b7e000 00000036 00000000 00360000

ff80: 00000001 00000000 c3b7e000 40024000 be8a465c c004b2fc c002706c c0027070

ffa0: 4013905c ffffffff fc400000 c0027bec 0000a2bd 40024894 05787df1 00000001

ffc0: 400248f0 00000000 00000000 00000003 af0fbe22 00000000 40024000 be8a465c

ffe0: be8a4690 be8a4598 400095b0 400090b8 20000010 ffffffff 804e5031 804e5431

[<c00b6f98>] (file_free_rcu+0x1c/0x64) from [<c0076120>] (__rcu_process_callbacks+0x224/0x2b4)

[<c0076120>] (__rcu_process_callbacks+0x224/0x2b4) from [<c00761c4>] (rcu_process_callbacks+0x14/0x38)

[<c00761c4>] (rcu_process_callbacks+0x14/0x38) from [<c004a6a0>] (__do_softirq+0xd4/0x1c8)

[<c004a6a0>] (__do_softirq+0xd4/0x1c8) from [<c004b2fc>] (irq_exit+0x44/0xa0)

[<c004b2fc>] (irq_exit+0x44/0xa0) from [<c0027070>] (_text+0x70/0x8c)

[<c0027070>] (_text+0x70/0x8c) from [<c0027bec>] (__irq_usr+0x4c/0x80)

 

Exception stack(0xc3b7ffb0 to 0xc3b7fff8)

ffa0:                                     0000a2bd 40024894 05787df1 00000001

ffc0: 400248f0 00000000 00000000 00000003 af0fbe22 00000000 40024000 be8a465c

ffe0: be8a4690 be8a4598 400095b0 400090b8 20000010 ffffffff

Code: e5903000 e3530000 ca000002 e3a03000 (e5833000)

Kernel panic - not syncing: Fatal exception in interrupt

 

Please help me....

タグ(1)
0 件の賞賛
返信
7 返答(返信)

4,286件の閲覧回数
汶颖谢
Contributor I

hi,have you solved this problem?

0 件の賞賛
返信

4,286件の閲覧回数
FlorentAuger
Contributor V

Hi,

 

Since the NAND and DDR2 parts are different, you have to adjust things compare to the default software config of the i.MX25 PDK.

The timings of the DDR2 can be slightly different, even if most of the time it's standard. So, you should take care of this.

That should indeed be into u-boot, I guess it's in the DCD table.

 

There's typically nothing but the support of the NAND to add into u-boot, which is its ID, size, bus width,...

Timings are not sensitive for that slow interface.

 

It seems that your design uses 2 DDR2. As the default Linux BSP is made for a single part, there are also things to adjust there. But I can help with that.

0 件の賞賛
返信

4,286件の閲覧回数
albert_arquer
Contributor I

Any thoughts?

0 件の賞賛
返信

4,286件の閲覧回数
albert_arquer
Contributor I

Hi, thanks for your replies.

 

Krishna, I am not sure what environment variables you are referring to. Are you talking about u-boot's variables, or linux's variables. How could an environment variable affect me this way?

 

Fabio, I don't have a MX25PDK available right now wo I can't test this on one.. .however, I would think it would work as I have not modified any source code or kernel configuration (I haven't added any drivers/modules etc.).

The differences between the two boards are mainly the Nand Flash and the SDRAM. In my board the models used are:

SDRAM: MT47H32M16 (two of them hanging from CS2 and CS3)

Nand Flash: HYNIX HY27UF084G2B-TPCB (hanging from the NFC)

 

Could the problem have to do with timing issiues? as I have noticed the errors are much less likely to occur once the board has been working for a while? If this were the case, how should I fix it? would it be a matter of modifying the configuration of the ESDRAM and NFC controllers in the u-boot code?

Is there any application note or document I could read?

 

Thanks a lot in advances

0 件の賞賛
返信

4,286件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Some suggestions:

 

1. Are you able to get this same crash on a MX25PDK?

 

2. When you say that your board is "almost identical" to MX25PDK: have you taken care of the changes in the bootloader and kernel?

0 件の賞賛
返信

4,286件の閲覧回数
KrishnaPavan
Contributor II
Are you sure that, the environment variables are set to be O.K? If not then they might be needing your attention.
0 件の賞賛
返信

4,286件の閲覧回数
albert_arquer
Contributor I

Please could someone just tell me where to start? this board is supposed to be part of and industrial design which needs to be on 24/7 so the eventual crashes are totally unacceptable for us....

 

Please help....

 

PS: I turned on Kernel debugging in the "kernel hacking section" and I removed the PHY driver support as our board does not have the RMII transciever solded on... The system keeps crashing all the time but now the board does not actually hang after the crash. After every "crash" I get the logging prompt "freescale login:".

0 件の賞賛
返信