kernel loading is not completing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kernel loading is not completing

1,487 Views
srinivasaporam
Contributor II

Hi,

We have got an freescale IMX6 board which designed based on reference deisgn. UBoot part is completed and and its loading the kernel.

 

But while loading it is checking for ethernet and stopping there for longer time ( not proceeding further).

 

 

 

Following are messages we are getting for reference board:

 

    [4.130762] using random self ethernet address                              

    [4.135228] using random host ethernet address                              

    [4.140310] usb0: HOST MAC 46:a0:19:68:95:15                                

    [4.144655] usb0: MAC 72:0b:10:7f:cb:bf                                     

    [4.148580] using random self ethernet address                              

    [4.153038] using random host ethernet address                              

    [4.157558] g_ether gadget: Ethernet Gadget, version: Memorial Day 2008     

    [4.164181] g_ether gadget: g_ether ready

 

Following are messages for custom board:

 

    [7.659608] using random self ethernet address                              

    [7.664068] using random host ethernet address                              

    [7.669096] usb0: HOST MAC ce:66:ce:41:ef:05                                

    [7.673434] usb0: MAC 16:f7:a4:5c:d2:82 

 

after this stage this is staying there itself for longer time and not progressing further

 

there might some problem with ethernet card (NIC) in our custom board.

what is problem how resolve this. Also find console messages for both reference board and custom board     

Original Attachment has been moved to: Reference_board_boot_messages.zip

Original Attachment has been moved to: custom_board_boot_messages.zip

Labels (2)
0 Kudos
Reply
1 Reply

1,404 Views
Yuri
NXP Employee
NXP Employee

Hello,

Please try to check memory using the DDR stress tool.

“i.MX6/7 DDR Stress Test Tool V2.20”

https://community.freescale.com/docs/DOC-105652


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply