kernel does not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kernel does not work

4,204 Views
zhangmike
Contributor II

Version:1.0 StartHTML:000000263 EndHTML:000030137 StartFragment:000002719 EndFragment:000030105 StartSelection:000002719 EndSelection:000030105 SourceURL:https://community.nxp.com/discussion/create.jspa?question=true&containerType=2020&containerID=134296

Hi;

My board is imx6q sabresd.

Enviroment: android9.0

My kernel starts in half and then stops.

log is here:

U-Boot 2018.03-dirty (Jul 04 2019 - 15:06:50 +0800)
CPU:   Freescale i.MX6Q rev1.3 996 MHz (running at 792 MHz)
CPU:   Automotive temperature grade (-40C to 125C) at 55C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: MX6-SabreSD
DRAM:  2 GiB
[2019-07-04 15:17:47.235]# RECV ASCII>
MMC:   FSL_SDHC: 0
Loading Environment from MMC...
[2019-07-04 15:17:47.385]# RECV ASCII>
*** Warning - bad CRC, using default environment
Failed (-5)
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In:    serial
Out:   serial
Err:   serial
flash target is MMC:0
[2019-07-04 15:17:47.569]# RECV ASCII>
Net:   No ethernet found.
[2019-07-04 15:17:47.994]# RECV ASCII>
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot:  3
[2019-07-04 15:17:48.987]# RECV ASCII>
2
[2019-07-04 15:17:49.995]# RECV ASCII>
1
[2019-07-04 15:17:50.984]# RECV ASCII>
0
[2019-07-04 15:17:51.031]# RECV ASCII>
RNG already instantiated 0x40000003
Error: blob decap job failed 0x2000081a
Error during blob decap operation: 0x2000081a
In boota get fastboot lock status error. Set lock status
RNG already instantiated 0x40000003
[2019-07-04 15:17:52.304]# RECV ASCII>
RNG already instantiated 0x40000003
 verify OK, boot 'boot'
[2019-07-04 15:17:52.413]# RECV ASCII>
kernel   @ 14008000 (9636992)
ramdisk  @ 15000000 (1835262)
fdt      @ 14f00000 (54498)
## Booting Android Image at 0x14007800 ...
Kernel load addr 0x14008000 size 9412 KiB
## Flattened Device Tree blob at 14f00000
   Booting using the fdt blob at 0x14f00000
   XIP Kernel Image ... OK
   Using Device Tree in place at 14f00000, end 14f104e1
switch to ldo_bypass mode!
Starting kernel ...

[2019-07-04 15:17:54.731]# RECV ASCII>
Booting Linux on physical CPU 0x0
Linux version 4.14.98-dirty (mikezhang@sileadinc) (gcc version 4.9.x 20150123 (prerelease) (GCC)) #2 SMP PREEMPT Wed Jul 3 16:33:09 CST 2019
CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
OF: fdt: Machine model: Freescale i.MX6 Quad SABRE Smart Device Board
Memory policy: Data cache writealloc
cma: Reserved 320 MiB at 0x2a000000
random: get_random_bytes called from start_kernel
[2019-07-04 15:17:54.744]# RECV ASCII>
+0xac/0x450 with crng_init=0
percpu: Embedded 18 pages/cpu @f64e6000 s41292 r8192 d24244 u73728
Built 1 zonelists, mobility grouping on.  Total pages: 522290
Kernel command line: console=ttymxc0,115200 init=/init video=mxcfb0:dev=ldb,fbpix=RGB32,bpp=32 video=mxcfb1:off video=mxcfb2:off video=mxcfb3:off vmalloc=128M androidboot.console=ttymxc0 consoleblank=0 androidboot.hardware=freescale cma=320M galcore.contiguousSize=33554432 loop.max_part=7 buildvariant=userdebug androidboot.serialno=201779d4df645324
[2019-07-04 15:17:54.752]# RECV ASCII>
androidboot.btmacaddr=20:17:79:d4:df:64 androidboot.soc_type=imx6q androidboot.storage_type=emmc androidboot.boottime=1BLL:0,1BLE:5441,KL:0,KD:0,AVB:921,ODT:0,SW:0 androidboot.bootreason=cold,powerkey androidboot.verifiedbootstate=green androidboot.slot_suffix= androidboot.vbmeta.device=PARTUUID=e88145d6-ce29-4767-84fb-5546bb954325 androidboot.vbmeta.avb_version=1.1 androidboot.vbmeta.device_state=locked androidboot.vbmeta.hash_alg=sha256 androidboot.vbmeta.size=2944 androidboot.vbmeta.digest=6b2b2d75679acf
[2019-07-04 15:17:54.765]# RECV ASCII>
9b12df70891f00a6db3b6f32b4ae5f6ffb759703b8b5179b0b androidboot.veritymode=enforcing androidboot.dtbo_idx=0 androidboot.keystor
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 1726304K/2097152K available (12288K kernel code, 990K rwdata, 3876K rodata, 1024K init, 501K bss, 43168K reserved, 327680K cma-reserved, 1187840K highmem)
Virtual kernel memory layout:
    v
[2019-07-04 15:17:54.778]# RECV ASCII>
ector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0xf8000000 - 0xff800000   ( 120 MB)
    lowmem  : 0xc0000000 - 0xf7800000   ( 888 MB)
    pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    modules : 0xbf000000 - 0xbfe00000   (  14 MB)
      .text : 0xc0008000 - 0xc0d00000   (13280 kB)
      .init : 0xc1200000 - 0xc1300000   (1024 kB)
      .data : 0xc1300000 - 0xc13f7bc8   ( 991 kB)
       .bss : 0xc13f9000 - 0xc1476780   ( 502 kB)
SLUB:
[2019-07-04 15:17:54.787]# RECV ASCII>
HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
ftrace: allocating 40331 entries in 119 pages
Preemptible hierarchical RCU implementation.
 Tasks RCU enabled.
NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
L2C-310 errata 752271 769419 enabled
L2C-310 enabling early BRESP for Cortex-A9
L2C-310 full line of zeros enabled for Cortex-A9
L2C-310 ID prefetch enabled, offset 16 lines
L2C-310 dynamic clock gating enabled, standby mode enabled
L2C-310 cache controller enabled, 16 ways, 1024 kB
L2C-3
[2019-07-04 15:17:54.798]# RECV ASCII>
10: CACHE_ID 0x410000c7, AUX_CTRL 0x76470001
Switching to timer-based delay loop, resolution 333ns
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
pid_max: default: 32768 minimum: 301
Security Framework initialized
SELinux:  Initializing.
Mou
[2019-07-04 15:17:54.809]# RECV ASCII>
nt-cache hash table entries: 2048 (order: 1, 8192 bytes)
Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
CPU: Testing write buffer coherency: ok
CPU0: Spectre v2: using BPIALL workaround
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x10100000 - 0x10100060
Hierarchical SRCU implementation.
smp: Bringing up secondary CPUs
[2019-07-04 15:17:55.077]# RECV ASCII>
 ...
CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
CPU1: Spectre v2: using BPIALL workaround
CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
CPU2: Spectre v2: using BPIALL workaround
CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
CPU3: Spectre v2: using BPIALL workaround
smp: Brought up 1 node, 4 CPUs
SMP: Total of 4 processors activated (24.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
CPU3: update max cpu_capacity 1024
devtmpfs: initialized
CPU2: update max cpu_capacity 1024
VFP su
[2019-07-04 15:17:55.089]# RECV ASCII>
pport v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
futex hash table entries: 1024 (order: 4, 65536 bytes)
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor menu
CPU identified as i.MX6Q, silicon rev 1.5
vdd1p1: supplied by regulator-dummy
vdd3p0: supplied by regulator-dummy
[2019-07-04 15:17:55.102]# RECV ASCII>
vdd2p5: supplied by regulator-dummy
vddarm: supplied by regulator-dummy
vddarm: failed to get the current voltage(-22)
anatop_regulator 20c8000.anatop:regulator-vddcore: failed to register vddarm
anatop_regulator: probe of 20c8000.anatop:regulator-vddcore failed with error -22
vddpu: supplied by regulator-dummy
vddsoc: supplied by regulator-dummy
vddsoc: failed to get the current voltage(-22)
anatop_regulator 20c8000.anatop:regulator-vddsoc: failed to register vddsoc
anatop_regulator: probe of 20c
[2019-07-04 15:17:55.114]# RECV ASCII>
8000.anatop:regulator-vddsoc failed with error -22
hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 4 bytes.
imx6q-pinctrl 20e0000.iomuxc: Invalid fsl,pins or pins property in node /soc/aips-bus@02000000/iomuxc@020e0000/gpio_leds/gpioledsgrp
imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
imx rpmsg driver is registered.
pstore: using zlib compression
console [pstore-1] enabled
pstore: Registered ramoops as persistent s
[2019-07-04 15:17:55.124]# RECV ASCII>
tore backend
ramoops: attached 0x100000@0x3ff00000, ecc: 0/0
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
usb_phy_generic 2000000.aips-bus:usbphy_nop1: 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
usb_phy_generic 2000000.aips-bus:usbphy_nop2: 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
i2c i2c-0: IMX I2C adapter registered
i2c i
[2019-07-04 15:17:55.135]# RECV ASCII>
2c-0: can't use DMA, using PIO instead.
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA, using PIO instead.
i2c i2c-2: IMX I2C adapter registered
i2c i2c-2: can't use DMA, using PIO instead.
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>
PTP clock support registered
imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
imx-ipuv3 2800000.ipu: IPU DMF
[2019-07-04 15:17:55.146]# RECV ASCII>
C NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 driver probed
mxc_mipi_csi2 21dc000.mipi_csi: i.MX MIPI CSI2 dphy version is 0x3130302a
MIPI CSI2 driver module loaded
Advanced Linux Sound Architecture Driver Initialized.
Bluetooth: Core ver 2.22
NET: Registered protocol family 31
Bluetooth: HCI device and connection manager initialized
Bluetooth: HCI socket layer initialized
Bluetooth: L
[2019-07-04 15:17:55.156]# RECV ASCII>
2CAP socket layer initialized
Bluetooth: SCO socket layer initialized
clocksource: Switched to clocksource mxc_timer1
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 3, 32768 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Has
[2019-07-04 15:17:55.355]# RECV ASCII>
h tables configured (established 8192 bind 8192)
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 1796K
hw perfevents: no interrupt-affinity property for /soc/pmu, guessing.
hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
Bus freq driver module loaded
audit: initializing netlink subsys (disabled)
audit: type=
[2019-07-04 15:17:55.368]# RECV ASCII>
2000 audit(0.700:1): state=initialized audit_enabled=0 res=1
workingset: timestamp_bits=14 max_order=19 bucket_order=5
Registering sdcardfs 0.1
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.26)
bounce: pool size: 64 pages
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
io scheduler mq-deadline registered
io scheduler kyber registered
pwm-backlight backlight: backlight supply power not found, using dummy regulator
[2019-07-04 15:17:55.380]# RECV ASCII>
mxc_mipi_dsi 21e0000.mipi: i.MX MIPI DSI driver probed
############################begin: set lcd power##########################
xxxxxxxxxldb_probe, line=710, lcd_tcon_en=39!
xxxxxxxxxldb_probe, line=724, mblpw=86!
ldb 2000000.aips-bus:ldb: xxxxxrequest mblpw gpio failed:-16
xxxxxxxxxldb_probe, line=738, dmipls=126!
############################end: set lcd power##########################
imx6q-pinctrl 20e0000.iomuxc: pin MX6Q_PAD_DISP0_DAT9 already requested by 2000000.aips-bus:ldb; cannot claim f
[2019-07-04 15:17:55.387]# RECV ASCII>
or lcd@0
imx6q-pinctrl 20e0000.iomuxc: pin-101 (lcd@0) status -22
imx6q-pinctrl 20e0000.iomuxc: could not request pin 101 (MX6Q_PAD_DISP0_DAT9) from group ipu1grp  on device 20e0000.iomuxc
mxc_lcdif lcd@0: Error applying setting, reverse things back
mxc_lcdif: probe of lcd@0 failed with error -22
mxc_sdc_fb fb@0: registered mxc display driver ldb
Console: switching to colour frame buffer device 100x30
mxc_sdc_fb fb@1: Can't get fb option for mxcfb1!
mxc_sdc_fb fb@2: Can't get fb option for mxcfb2!
[2019-07-04 15:17:55.398]# RECV ASCII>
mxc_sdc_fb fb@3: Can't get fb option for mxcfb3!
imx-sdma 20ec000.sdma: no iram assigned, using external mem
imx-sdma 20ec000.sdma: Falling back to user helper
mxs-dma 110000.dma-apbh: initialized
imx-pgc-pd imx-pgc-power-domain.0: Linked as a consumer to 20dc000.gpc
imx-pgc-pd imx-pgc-power-domain.1: Linked as a consumer to 20dc000.gpc
i2c i2c-1: SCL is stuck low, exit recovery
pfuze100-regulator 1-0008: unrecognized pfuze chip ID!
pfuze100-regulator: probe of 1-0008 failed with error -11
2020000.
[2019-07-04 15:17:55.415]# RECV ASCII>
serial: ttymxc0 at MMIO 0x2020000 (irq = 27, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 73, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized vivante 1.0.0 20120216 for platform:Vivante GCCore on minor 0
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
zram: Added device: zram0
[2019-07-04 15:17:55.534]# RECV ASCII>
libphy: Fixed MDIO Bus: probed
tun: Universal TUN/TAP device driver, 1.6
CAN device driver interface
fec 2188000.ethernet: 2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: f2:d9:d7:f9:d6:34
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
PPP
[2019-07-04 15:17:55.550]# RECV ASCII>
generic driver version 2.4.2
PPP BSD Compression module registered
PPP Deflate Compression module registered
PPP MPPE Compression module registered
usbcore: registered new interface driver kaweth
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver
usbcore: registered new interface driver pegasus
usbcore: registered new interface driver rtl8150
usbcore: registered new interface driver r8152
usbcore: registered new interface driver asix
usbcore: registered new interface driver ax881
[2019-07-04 15:17:55.562]# RECV ASCII>
79_178a
usbcore: registered new interface driver cdc_ether
usbcore: registered new interface driver net1080
usbcore: registered new interface driver cdc_subset
usbcore: registered new interface driver zaurus
usbcore: registered new interface driver cdc_ncm
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
usbcore: registered new interface driver usb_ehset_test
usbmisc_imx 2184800.usbmisc: 218
[2019-07-04 15:17:55.625]# RECV ASCII>
4800.usbmisc supply vbus-wakeup not found, using dummy regulator
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
usb
[2019-07-04 15:17:55.656]# RECV ASCII>
usb1: New USB device found, idVendor=1d6b, idProduct=0002
usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
usb usb1: Product: EHCI Host Controller
usb usb1: Manufacturer: Linux 4.14.98-dirty ehci_hcd
usb usb1: SerialNumber: ci_hdrc.1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
usbcore: registered new interface driver xpad
usbcore: registered new interface driver usb_acecad
usbcore: registered new interface driver aiptek
usbcore: registered new interface driver gtco
u
[2019-07-04 15:17:55.701]# RECV ASCII>
sbcore: registered new interface driver hanwang
usbcore: registered new interface driver kbtab
<<-GTP-INFO->> GTP driver installing...
<<-GTP-INFO->> GTP Driver Version: V2.2<2014/01/14>
<<-GTP-INFO->> GTP I2C Address: 0x5d
<<-GTP-INFO->> Guitar reset
[2019-07-04 15:17:55.873]# RECV ASCII>
<<-GTP-INFO->> IC Version: 911_1060
<<-GTP-INFO->> X_MAX: 0, Y_MAX: 0, TRIGGER: 0x00
[2019-07-04 15:17:55.958]# RECV ASCII>
<<-GTP-INFO->> create proc entry gt9xx_config success
input: goodix-ts as /devices/virtual/input/input0
gpio gpiochip4: (20ac000.gpio): gpiochip_lock_as_irq: tried to flag a GPIO set as output for IRQ
gpio-mxc 20ac000.gpio: unable to lock HW IRQ 6 for IRQ
genirq: Failed to request resources for gd111x (irq 216) on irqchip gpio-mxc
<<-GTP-ERROR->> Request IRQ failed!ERRNO:-22.
<<-GTP-INFO->> GTP works in polling mode.
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-rtc-lp as
[2019-07-04 15:17:55.970]# RECV ASCII>
rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
mxc_v4l2_output v4l2_out: V4L2 device registered as video16
mxc_v4l2_output v4l2_out: V4L2 device registered as video17
[2019-07-04 15:17:56.005]# RECV ASCII>
ov564x 0-003c: cannot get io voltage
ov564x 0-003c: cannot get core voltage
ov564x 0-003c: cannot get analog voltage
[2019-07-04 15:17:56.177]# RECV ASCII>
ov5640_read_reg:write reg error:reg=300a
camera ov5640 is not found
ov5642_power_on: cannot get io voltage error
ov5642_power_on: cannot get core voltage error
ov5642_power_on: cannot get analog voltage error
[2019-07-04 15:17:56.322]# RECV ASCII>
ov5642_read_reg:write reg error:reg=300a
camera ov5642 is not found
ov5640_power_on: cannot get io voltage error
ov5640_power_on: cannot get core voltage error
ov5640_power_on: cannot get analog voltage error
[2019-07-04 15:17:56.645]# RECV ASCII>
i2c i2c-1: SCL is stuck low, exit recovery
ov5640_read_reg:write reg error:reg=300a
camera ov5640_mipi is not found
usbcore: registered new interface driver uvcvideo
USB Video Class driver (1.1.1)
__power_supply_register: Expected proper parent device for 'battery'
(NULL device *): hwmon_device_register() is deprecated. Please convert the driver to use hwmon_device_register_with_info().
__power_supply_register: Expected proper parent device for 'usb'
mag3110 2-000e: check mag3110 chip ID
mag3110 2-
[2019-07-04 15:17:56.656]# RECV ASCII>
000e: read chip ID 0xfffffff5 is not equal to 0xc4!
mag3110: probe of 2-000e failed with error -22
mma8x5x 0-001c: read chip ID 0xfffffffa is not equal to 0x1a,0x2a,0x3a,0x4a,0x5a!
mma8x5x: probe of 0-001c failed with error -22
imx2-wdt 20c0000.wdog: timeout 60 sec (nowayout=0)
device-mapper: uevent: version 1.0.3
device-mapper: ioctl: 4.37.0-ioctl (2017-09-20) initialised: [email protected]
Bluetooth: HCI UART driver ver 2.3
Bluetooth: HCI UART protocol H4 registered
Bluetooth: HCI UART protocol
[2019-07-04 15:17:56.705]# RECV ASCII>
 BCSP registered
Bluetooth: HCI UART protocol ATH3K registered
bt power gpio is:2
rfkill: BT RF going to : on
mxc_bt_rfkill_reset
mxc_bt_rfkill driver success loaded
usbcore: registered new interface driver btusb
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
[2019-07-04 15:17:56.781]# RECV ASCII>
mmc0: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
mxc_vpu 2040000.vpu_fsl: VPU initialized
mxc_hdmi_cec soc:hdmi_cec@00120000: HDMI CEC initialized
Galcore version 6.2.4.190076
[2019-07-04 15:17:56.828]# RECV ASCII>
mmc0: new DD
[2019-07-04 15:17:56.887]# RECV ASCII>
R MMC card at address 0001
mmcblk0: mmc0:0001 MMC08G 7.25 GiB
mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
mmcblk0rpmb: mmc0:0001 MMC08G partition 3 128 KiB
Alternate GPT is invalid, using primary GPT.
 mmcblk0: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13
Labels (4)
0 Kudos
Reply
3 Replies

3,908 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhang

one can try Demo Image and follow sect.3.3 Flashing board images attached Android Quick Start Guide

Demo Images – i.MX 6Quad, i.MX 6QualPlus, and i.MX 6DualLite SABRE-SD Boards and Platforms

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,908 Views
zhangmike
Contributor II

Hi  Igorpadykov:

    Please help me.

zhang mike

0 Kudos
Reply

3,908 Views
zhangmike
Contributor II

Hi igorpadykov:

    When I use uuu_imx_android_flash.sh script to flash the demo Images, it issue.

S2SE5V~4.PNG

0 Kudos
Reply