Hi,
I configured all peripehricals / IO into u-boot.
I know there is the possibility to call the number 0x80000000 into kernel to get the previous setting:
for example
&iomuxc {      pinctrl-names = "default";      pinctrl-0 = <&pinctrl_hog>;       hog {           pinctrl_hog: hoggrp {           fsl,pins = <                 /* gpio-leds */                MX6QDL_PAD_EIM_D28__GPIO3_IO28 0x80000000                MX6QDL_PAD_EIM_A25__GPIO5_IO02 0x80000000                 /* J11 pins 32, 34, 36, 38 */                MX6QDL_PAD_CSI0_DAT8__GPIO5_IO26     8                MX6QDL_PAD_CSI0_DAT9__GPIO5_IO27     8                MX6QDL_PAD_KEY_COL1__GPIO4_IO08          8                MX6QDL_PAD_KEY_ROW1__GPIO4_IO09          8           >;           };      }; };In this way, i avoid to configure again the IO.
What do you suggest?
To configure all pin into u-boot and after to call 0x80000000 for all IO into kernel, or to configure again?
What is it the correct procedure?
thank you
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Fausto
you are right, according to linux/Documentation/devicetree/bindings/pinctrl/fsl,imx-pinctrl.txt :
Bits used for CONFIG:
NO_PAD_CTL(1 << 31): indicate this pin does not need config. 
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok,
what is the best practice?
To set all peripherals into u-boot and after to call NO_PAD_CTL(1 << 31)?
Thanks
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		I believe both options are acceptable.
Best regards
igor