it6251

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

it6251

3,184 Views
yuhundehao
Contributor III

Board:imx6q

linux kernel :3.0.35 

I want to use it6251 conversion chip to convert LVDS signal into EDP signal. Now the conversion is successful, but there is a problem that the logo display interface is not displayed, and the app startup interface can be displayed normally,why?

I can't even try to initialize the chip by putting it into uboot。

Labels (3)
0 Kudos
Reply
2 Replies

3,082 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuhundehao

one can try to adjust lvds timing parameters in struct fb_videomode using example on

IMX6Q drive the LVDS screen ,but can not light up... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,082 Views
yuhundehao
Contributor III

Thanks ! 

I solve . Because The reset foot of it6251 is pulled down

0 Kudos
Reply