it6251

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

it6251

3,204件の閲覧回数
yuhundehao
Contributor III

Board:imx6q

linux kernel :3.0.35 

I want to use it6251 conversion chip to convert LVDS signal into EDP signal. Now the conversion is successful, but there is a problem that the logo display interface is not displayed, and the app startup interface can be displayed normally,why?

I can't even try to initialize the chip by putting it into uboot。

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

3,102件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Yuhundehao

one can try to adjust lvds timing parameters in struct fb_videomode using example on

IMX6Q drive the LVDS screen ,but can not light up... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,102件の閲覧回数
yuhundehao
Contributor III

Thanks ! 

I solve . Because The reset foot of it6251 is pulled down

0 件の賞賛
返信