issue about imx6 uart dma

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

issue about imx6 uart dma

10,961 Views
宗標廖
Contributor V

Hello Community

My customer uses BSP3.0.35_4.1.0 on i.mx6dl and they connected BT to UART4, and they enabled SDMA for UART4.

They found that when the BT chip is communicating with i.MX6, sometimes the Rx DMA of UART4 goes to stop. 

Could you give me some advice to resolve this problem?

Best Regards

ZongbiaoLiao

Labels (2)
0 Kudos
Reply
5 Replies

9,923 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

please check attached Linux Manual Chapter 39
Universal Asynchronous Receiver/Transmitter (UART) Driver

If you want to use the DMA support for UART please also
enable the RTS/CTS for it. The DMA may be abnormal if you
do not enable the RTS/CTS.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

9,923 Views
宗標廖
Contributor V

Hi igor

Thank you for you reply.

My customer used CTS/RTS. So is there any other possible reason?

Best Regards

ZongbiaoLiao

0 Kudos
Reply

9,921 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

since L3.0.35 uart driver was significantly changed, for example

refer to attached patches. So recommendation to migrate to more new kernels.

Best regards
igor

0 Kudos
Reply

9,921 Views
宗標廖
Contributor V

Hi igor

Thank you for offer me patches.

My customer's project is based on L3.0.35_4.1.0, now it is impossible(no time) to migrate to newer BSP.

Best Regards

ZongbiaoLiao

0 Kudos
Reply

9,921 Views
igorpadykov
NXP Employee
NXP Employee

Hi ZongbiaoLiao

L3.0.35_4.1.0 is old bsp and not supported in usual way,

it is removed from nxp bsps software page

i.MX 6 / i.MX 7 Series Software and Development Tool|NXP 

 its support provided by NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards
igor

0 Kudos
Reply