ip camera interfacing with mimxrt1170

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ip camera interfacing with mimxrt1170

1,031 Views
sandeep_c
Contributor I

hi everyone 

i need to interface ip camera with rt1170 processor by using LWIP stack with rtp protocol 

ip camera: DH-IPC-MBW4231-AS/M12 ( rj45 ethernet type)

camera datasheet: https://www.dahuasecurity.com/products/productDetail/14801

supported protocols by camera: HTTP; HTTPs; TCP; ARP; RTSP; RTP; UDP; SMTP;FTP; DHCP; DNS; DDNS; PPPOE; IPv4/v6; QoS;UPnP;NTP; Bonjour;802.1x; Multicast; ICMP;IGMP; SNMP

Proocessor : mimxrt1170

IDE: MCUXpresso IDE v11.6.0 [Build 8187] [2022-07-13] using on windows not linux

physical layer: rj45 ethernet type

by using above resources i need stream a video if any knows the how to stream video or any tools to analyze the data and as well how can i implement this

 

can we use embedded wizard? if yes how can i use it or what extension formt of video?

how can i approach to this problem

 

 

 

0 Kudos
Reply
0 Replies