interrupt not capturing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

interrupt not capturing

1,401件の閲覧回数
mathew_k_t
Contributor II

Hi,

I'm using an imx6ull board.

I implemented a new SPI device driver in it. That driver contains a diagnostic interrupt, which checks for faults before initialization of the device.

The interrupt is a GPIO interrupt. So I implemented as follows,

adc->diag_irq = gpio_to_irq(6);

ret = devm_request_irq(adc->dev, adc->diag_irq, diagnostic_handler, IRQF_TRIGGER_RISING, "DIAG_END", 0);

I implemented this in the driver probe() and immediately enabled start diagnostics bit.

Once the bit is set, within 8mesc it receives diag_end interrupt. It is a one time process before initialization of the device.

But the processor doesn't read the interrupt. The diagnostic check and device initialization are done in the probe() only.

I manually gave interrupt. That time I found my ISR is working. Which means, the interrupt implementation and ISR registrations are working.

Why is it not receiving the interrupt? Any timing issue like debouncing.

Could you suggest a solution to solve this issue?

Regards

ラベル(3)
0 件の賞賛
返信
0 返答(返信)