interlaced data capture issues on imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

interlaced data capture issues on imx6q

1,491 次查看
lsg5131420
Contributor III

hi

I used adv7611 capture vedio on imx6q platfrom.and i can received 1080p vedio corectly. but when capture the 1080i vedio data, the vedio displaying from top to bottom quickly. the code i only modifed is  setting the clk_mode to IPU_CSI_CLK_MODE_CCIR1120_INTERLACED_SDR.

Anything wrong with the code setting and How can i do next?

Thanks!

0 项奖励
回复
1 回复

1,227 次查看
igorpadykov
NXP Employee
NXP Employee

Hi shiguang

please check interlaced patches on

iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP 

iMX6 camera patch to support CSI->VDI->IC->MEM and CSI->VDI->MEM capture 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复