install any library in yocto

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

install any library in yocto

2,527件の閲覧回数
senthilkumar_s1
Contributor II

Hello,

          I am working on i.mx6Quad Sabre-SD with YOCTO environment(poky and jethro versions).

          I am facing problems while making few library files present on target(i.mx6)Ex. (sox,swig,bison,awk,python-pyaudio etc)

          Either of these two ways will be helpful

          1.Making apt-get install work on Yocto environment{Installed apt,But proper sources.list is not present}

          2.Any other way to install those library packages

Or else recommendation of any other flavours(like jethro) where I can easily deploy those header files is also appreciated

Thank You in Advance

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,848件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Senthil Kumar,

You should be able to add apt on all of the Yocto branches, certainly in Jethro. Installing apt does not configure it to reach any servers, as far as I know. It is not setup. So what you saw is correct, you would need to add the list of repositories from which apt would look for new libraries or packages.

There is some information about package management on the following document, although it’s not apt oriented it may serve as some concepts are similar.

https://community.nxp.com/docs/DOC-328199

The following wiki has information on the sources.list file for apt.

https://wiki.debian.org/SourcesList

I hope this helps! Please let us know of your findings!

Regards,

0 件の賞賛
返信