initialization code of Enhanced SDRAM Controller (i.MX51 WEC7)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

initialization code of Enhanced SDRAM Controller (i.MX51 WEC7)

1,229 Views
eishishibusawa
Contributor III

Dear Sir

 

I want to ask about initialization code of Enhanced SDRAM Controller (eSDCTL).

I cannot find the init code in WEC7 BSP for i.MX51.

Which source file of i.MX51 WEC7 BSP contains the init code?

 

Best Regards,

Eishi SHIBUSAWA

 

Labels (2)
0 Kudos
Reply
1 Reply

1,132 Views
igorpadykov
NXP Employee
NXP Employee

Hi Eishi

please check

WEC7/PLATFORM/iMX51_EVK/SRC/BOOTLOADER/EBOOT/flash_header.s

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply