information on sources and abilities of i.MX6q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

information on sources and abilities of i.MX6q

Jump to solution
1,439 Views
synthnassizer
Contributor III

Hello everyone,

I am thinking of buying an Element14 Sabre lite development board.

I am abit fuzzy as to how much of the development board has been set up by Element14 and how much by Freescale itself; are there drivers (or anything else) that is not supported by the sources/images found in the link down below?

Also, are there board characteristics that are enabled in the image files, but which I can not compile in from the sources?

is this link with SDK, linux OS (or android), correct?

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&nodeId=018rH3ZrDRB24A&fpsp=1&t...

A few comments refering to the link above:

-Is the SDIOWORX non-GPL run-time driver necessary for writing to the SD card?

-LEIMX linux is mostly a busybox executable placed within a rootfs

Also

-I don't see any uboot sources. Should I assume I can refer to linaro toolchain and info about that?  http://www.element14.com/community/message/66325#66325/l/linaro-sabre-lite-resources

If you have links and discussion on the boarda please refer me to them. Searching the element14 and freescale websites refer me to little technical discussions, and google about the board provides alot of links from a sabre-lite implementation by boundary devices - which I am not certain if it is the same board.

Thank you very much for your help!


Labels (2)
0 Kudos
Reply
1 Solution
1,161 Views
jimmychan
NXP TechSupport
NXP TechSupport

The BSP is board specific. We have i.MX6-Sololite, i.MX6-SDB (Smart Device Board), i.MX6-SDP (Smart Device Platform) and i.MX6-AI (Automotive). You can download the corresponding BSP from here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

For the one you mentioned, I think you may go here:

http://boundarydevices.com/products/

View solution in original post

0 Kudos
Reply
1 Reply
1,162 Views
jimmychan
NXP TechSupport
NXP TechSupport

The BSP is board specific. We have i.MX6-Sololite, i.MX6-SDB (Smart Device Board), i.MX6-SDP (Smart Device Platform) and i.MX6-AI (Automotive). You can download the corresponding BSP from here:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW

For the one you mentioned, I think you may go here:

http://boundarydevices.com/products/

0 Kudos
Reply