incorrect cfg-File for imx8mn_ddr4_evk?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

incorrect cfg-File for imx8mn_ddr4_evk?

1,056件の閲覧回数
klaus_dannecker
Contributor I

Hi,

the Evalboard imx8mn_ddr4_evk has ddr4 ram (no lpddr4)

in the imx8mn_ddr4_evk_defconfig is referred to arch/arm/mach-imx/imx8m/imximage.cfg File

in this File is config plddr4 and not ddr4

..

DDR_FW lpddr4_pmu_train_1d_imem.bin
DDR_FW lpddr4_pmu_train_1d_dmem.bin
DDR_FW lpddr4_pmu_train_2d_imem.bin
DDR_FW lpddr4_pmu_train_2d_dmem.bin

..

is that correct?

or should another file be used, like imximage_ddr4.cfg?

that used

DDR_FW ddr4_imem_1d.bin
DDR_FW ddr4_dmem_1d.bin
DDR_FW ddr4_imem_2d.bin
DDR_FW ddr4_dmem_2d.bin

Sourcecode : https://source.codeaurora.org/external/imx/uboot-imx branch imx_v2019.04_4.19.35_1.1.0

Regards

Klaus

ラベル(1)
0 件の賞賛
返信
1 返信

960件の閲覧回数
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please note that the i.MX 8MN is still not supported in that release, for i.MX 8MN please use L4.14.98_2.3.0.

From L4.19.35_1.1.0
 pastedImage_2.png

 

Thank you,

Regards,

Aldo.

0 件の賞賛
返信