Hi all,
I'm using imx8qm with MEK.
I found NXP supports imx-gst1.0-plugins from Code Aurora git repositories
But I couldn't build it.
Could you guide me how can I build and test it? I want to add customization at imxvideoconvert_g2d plug-in.
I installed meson and ninja in my IMX8QM board.
Thanks,
Dongjin Ha.
Solved! Go to Solution.
why don't you use nxp yocto or standalone kernel? which includes all of gstreamer plugins already, you can refer to the Chapter 2 Porting Kernel of enclosed file
as my understanding, imx-gst1.0-plugins is a software run in user-space, rather than in kernel.
we can build the kernel standalone. Can we also build the imx-gst1.0-plugins separately?
In fact, we generate the rootfs with Buildroot.But I can't figure out how to build imx-gst1.0-plugins in buildroot. So I hope to build imx-gst1.0-plugins standalone and copy them into the rootfs.
yes, this isn't belong to the kernel, nxp yocto bsp includes this, this is source code link, maybe you can download it and build it
"https://github.com/nxp-imx/imx-gst1.0-plugin/tree/MM_04.07.00_2205_L5.15.y"
thanks @joanxie for your reply.
Do you have any tutorial about how to build https://github.com/nxp-imx/imx-gst1.0-plugin/tree/MM_04.07.00_2205_L5.15.y ?
It seems there is no detail info in its README
when I try to enter below command I can see below error.
mkdir build
cd build
meson ..
.....
../meson.build:22:0: ERROR: Dependency "gstreamer-1.0" not found, tried pkgconfig and cmake
why don't you use nxp yocto or standalone kernel? which includes all of gstreamer plugins already, you can refer to the Chapter 2 Porting Kernel of enclosed file