imxvideoconvert plug-in build guide

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

imxvideoconvert plug-in build guide

跳至解决方案
8,661 次查看
dongjin
Contributor II

Hi all,

 

I'm using imx8qm with MEK.

I found NXP supports imx-gst1.0-plugins from Code Aurora git repositories 

But I couldn't build it.

Could you guide me how can I build and test it? I want to add customization at imxvideoconvert_g2d plug-in.

I installed meson and ninja in my IMX8QM board.

 

Thanks,

Dongjin Ha.

0 项奖励
回复
1 解答
8,546 次查看
joanxie
NXP TechSupport
NXP TechSupport

why don't you use nxp yocto or standalone kernel? which includes all of gstreamer plugins already, you can refer to the Chapter 2 Porting Kernel of enclosed file

在原帖中查看解决方案

0 项奖励
回复
5 回复数
8,044 次查看
imx8-mdt
Contributor I

@joanxie

as my understanding,  imx-gst1.0-plugins is a software run in user-space, rather than in kernel.

we can build the kernel standalone. Can we also build the imx-gst1.0-plugins separately?

In fact,  we generate the rootfs with Buildroot.But I can't figure out how to build imx-gst1.0-plugins in buildroot. So I hope to build imx-gst1.0-plugins standalone and copy them into the rootfs.

 

 

0 项奖励
回复
8,033 次查看
joanxie
NXP TechSupport
NXP TechSupport

yes, this isn't belong to the kernel, nxp yocto bsp includes this, this is source code link, maybe you can download it and build it

"https://github.com/nxp-imx/imx-gst1.0-plugin/tree/MM_04.07.00_2205_L5.15.y"

0 项奖励
回复
8,030 次查看
imx8-mdt
Contributor I

thanks @joanxie for your reply.

Do you have any tutorial about how to build https://github.com/nxp-imx/imx-gst1.0-plugin/tree/MM_04.07.00_2205_L5.15.y ?  

It seems there is no detail info in its README

0 项奖励
回复
8,651 次查看
dongjin
Contributor II

when I try to enter below command I can see below error.

 

mkdir build

cd build

meson ..

 

.....

../meson.build:22:0: ERROR: Dependency "gstreamer-1.0" not found, tried pkgconfig and cmake

0 项奖励
回复
8,547 次查看
joanxie
NXP TechSupport
NXP TechSupport

why don't you use nxp yocto or standalone kernel? which includes all of gstreamer plugins already, you can refer to the Chapter 2 Porting Kernel of enclosed file

0 项奖励
回复