imxvideoconvert_ipu Gstreamer plugin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxvideoconvert_ipu Gstreamer plugin

2,437 Views
nissim_beja
Contributor I

Dear all,

I am using Variscite's DART-MX8M-MINI platform, running Yocto Sumo (i.e. sumo-fsl-4.14.98-mx8mm-v2.2)

I would like to test some features that combines a prosperity algorithm with gstreamer elements.

For that matter i would like to use the "imxvideoconvert_ipu" plugin. 

Unfortunately the "imxvideoconvert_ipu"  cannot be found (only imxvideoconvert_g2d was found).

Please advise which imx-gstreamer repository and brach should i use in order to be able using the imxvideoconvert_ipu 

Regards, 

Nissim.

0 Kudos
Reply
2 Replies

2,352 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Nissim,

The i.MX8 does not have IPU that the reason you can find the imxvideoconverter_ipu, this is for the i.MX6, you need to use imxvideoconverter_g2d.

Regards

0 Kudos
Reply

2,352 Views
nissim_beja
Contributor I

Hi,

Thanks, for your quick response.

The "i.MX Linux® Release Notes, Rev. L4.19.35_1.1.0, 11/2019" document doesn't mention that its only for I.MX6.

Let me suggest to update the document.

0 Kudos
Reply